The settings for frequency parameters can be changed in several ways:
From the Frequency Tab:
Click
To set
Frequency or Frequency , be sure that the Show Center/Span check box is selected. To set or Frequency, be sure that the Show Center/Span check box is cleared.Click the parameter to change (for example, Center).
Type the new value and press Enter or click Close.
From the Copy Marker to menu:
Click Markers > Copy Marker to, and the appropriate selection from the menu (Copy Mkr to Center Freq, for example).
From the Trace popup menu
Right-click in the trace.
From the popup menu, click Copy Mkr to Center Freq.
Using the Select Area tool
From the popup menu, click the appropriate selection (for example, Frequency
and ).
Copyright © 2000-2023 Keysight Technologies, Inc. |