An I+jQ logical VSA input channel measures data from two instrument channels where one channel supplies the real component of the data (I, or In-phase) and the other channel supplies the imaginary component (Q, or Quadrature-phase). The VSA supports up to 8 instrument channels for an Analyzer Configuration. Since each I+jQ logical input channel requires two instrument channels, there are four possible I+jQ selections: Single, Dual, Triple, or Quad I+jQ.
To view the default instrument channel assignment, select one of the I+jQ channel configurations, and then select
.For connections to specific measurement hardware, see Available Measurement Hardware for a link to your specific hardware.
There are several applications for the I+jQ input mode, including the following:
See Setting up a Digital Demodulation Measurement to learn how to use I+jQ for Digital Demodulation Measurements.
RF measurements can be made using an external quadrature downconverter by connecting the I/Q outputs to 2 channel baseband measurement hardware. "External" refers to measurement hardware that is not controlled by the VSA--for example, an Keysight 71910A Wideband Receiver with I and Q outputs. The measurement and configuration settings used by the external quadrature downconverter are input to the VSA using External Frequency Calibration.
Use either theCouple Paired Channels checkbox to synchronize all the range and coupling settings for active channels. will couple all channels together (for example, for Dual I+jQ (C1+jC2, C3+jC4), all four channels will be coupled with together). couples I and Q channels for each VSA channel (for example, for Dual I+jQ (C1+jC2, C3+jC4), VSA Channels 1 and 2 are coupled together and are independent of VSA Channels 3 and 4, which are also coupled together).
selection when adjusting range and coupling or select theSignals that are recorded in I+jQ mode should be played back in I+jQ mode. While they can be played back as 2 or 4 separate channels, the time corrections will not, in general, be consistent. 2-channel Baseband recordings, however, can be played back in I+jQ mode and time corrections will be accurate.
See Also
I+jQ Frequency Spectrum (Channels)
I+jQ Span and Frequency Information (Channels)
I+jQ Measurement Tips (Channels)
Copyright © 2000-2023 Keysight Technologies, Inc. |