The 5G NR Demod Properties dialog box lets you configure the decoding type, depending on the DL-BWP/UL-BWP selection. For downlink (DL-BWP), you can decode the PBCH, PDCCH and PDSCH. For uplink (UL-BWP), you can decode the PUCCH and PUSCH. For PDSCH and PUSCH, you can also select the decoding algorithm. The decoding results are shown in the Decoded Info and Decoded Symbols traces. CRC pass/fail results are also shown in the Slot Summary trace.
tab of theDepending on the complexity and length of the 5G NR signal, enabling decoding may affect the performance of your measurement. The following is recommended for improved speed when decoding is enabled:
The Decode tab has the following parameters and selections:
Decode Settings
Decode Advanced Settings
See Also
5G NR Demod Properties Dialog Box
Copyright © 2000-2023 Keysight Technologies, Inc. |