Menu Path:
The
dialog box contains parameters that let you configure the VSA to demodulate 5G NR signals.The 5G NR demodulator must be selected before this dialog box is available. To enable the demodulator, click
The
dialog box contains tab headings that group similar configuration parameters as follows:Configuration Tab: Contains the signal formatting parameters to configure the demodulator to match the 5G NR signal to be demodulated.
Input & Antenna Tab: Contains parameters that configure the antenna group to shape the signal's beam pattern.
Time Tab: Contains parameters that specify what part of the signal to analyze.
Decode Tab: Contains decode parameters.
Advanced Tab: Contains signal adjustment and correction parameters.
See Also
Setting up a 5G NR Measurement
Copyright © 2000-2023 Keysight Technologies, Inc. |