There are two types of traces in the Trace > Data > Demod and MIMO menus that display component carrier data: CCn (component carrier is fixed), and Selected Display CC (component carrier is dynamically selected using the Display parameter). See About Per-Carrier Trace Types for more information.
The Measurement Interval, organized into BWP/subframe/slot groupings.
trace shows the reference component carrier's summary data for the channels that are present in theSlot Summary is a type of Matrix Table that provides selectable column visibility and copy/paste and export functionality to share rows of content or complete tables to applications like email, text editing or spreadsheet programs.
Not visible by default To make visible, right-click any column heading and select Column Visibility... |
Not visible by default To make visible, right-click any column heading and select Column Visibility... |
||||||||||||||||||
---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|
BWP / Frame / Sf / Slot / Mu | Channel Name | BWP ID | Subframe Index | Slot Index | RNTI | Physical Channel | User | Part | Layer | EVM (%rms) | SINR (dB) | Power per RE (dBm) | Power Boosting (dB) | Modulation | Num. of RBs | CRC | Error Bits | Total Bits | BER (%) |
BWP / Frame / Sf / Slot / Mu displays BWP ID, Frame Index, Subframe Index, Slot Index and Numerology Index (displayed as "Mun"), grouped by slot. For the SSB channel, "SSB" is displayed instead of BWP ID. |
Channel Name is a unique, but arbitrary reference to a Slot Summary row that is derived from Physical Channel, User, Part and Layer as applicable. Possible names include: Downlink: Uplink:
|
BWP ID displays the ID number (or name) of the bandwidth part that is associated with the row's channel. The same value is shown in the "BWP" field within the BWP / Sf / Slot column. |
Subframe Index displays the channel's subframe index. The same value is shown in the "Sf" field within the BWP / Sf / Slot column. |
Slot Index displays the channel's slot index. The same value is shown in the "Slot" field within the BWP / Sf / Slot column. |
RNTI shows the Radio Network Temporary Identifier (RNTI) for the channel. |
Physical channels include:
PSS SSS PBCH PDCCH PDSCH PUCCH PUSCH CSI-RS DC |
When there is a single user, the default user number is 0. Rows without user data are denoted with '***'. |
Some physical channels have multiple parts. Physical channel parts include:
Data DMRS PTRS |
Rows without layer data are denoted with '***'. |
EVM is the per-layer RMS EVM after demodulation. The Report EVM in dB parameter affects the units of this data result. |
SINR is the signal-to-noise and interference ratio for the channel. |
Power is the per-subcarrier power received at the reference measurement channel, averaged over all the subcarriers belonging to the physical channel. |
Power Boosting is the amount of power boosting applied to the channel using the channel's Power Boosting parameter. |
Mod. Fmt. is the modulation format of the channel. The modulation format for Non-alloc signals is not shown.
BPSK_45Deg QAM16 QAM64 QAM256 BPSK_PI/2 Z-Chu |
Num. of RBs shows the number of resource blocks (1 RB x 1 slot) within the Measurement Interval that contain subcarriers belonging to the channel. Num. of RBs is not shown for Non-alloc signals. |
CRC displays the CRC pass/fail result for channels that are decoded. See Decode Tab for more information. Rows with channels that are not decoded are denoted with '***'. Decodable channels include:
PBCH PDCCH PDSCH PUCCH PUSCH |
Error Bits displays the detected per-slot bit errors. Bit Error Rate calculations are perfomed only for Downlink and when PDSCH IQ Ref is set to something other than Demod. |
Total Bits displays the total number of bits per slot used in BER calculation. Bit Error Rate calculations are perfomed only for Downlink and when PDSCH IQ Ref is set to something other than Demod. |
BER displays the per-slot calculated Bit Error Rate. Bit Error Rate calculations are perfomed only for Downlink and when PDSCH IQ Ref is set to something other than Demod. |
A multi-color coding scheme is used to make it easy to visually identify common symbols, subcarriers, and data results within various OFDM Traces. This makes cross trace data comparisons and analysis easier to accomplish. Different colors are assigned to symbols representing elements including: PSS/SSS/PBCH/PBCH_DMRS/PDSCH/PDSCH_DMRS/PUSCH/PUSCH_DMRS/PUCCH/PUCCH_DMRS. Some common color scheme Traces include: Error Vector Spectrum, Error Vector Time, OFDM Meas, Frame Summary and Slot Summary trace data.
The 5G NR color scheme has been simplified to help make visual sense of a complex standard. The default color assignment for 5G NR follows these general guidelines:
You can also customize and re-assign Trace colors schemes, see the Display Preferences Color tab (click tab and select a new color for the active Mod Type element).
See Also
Copyright © 2000-2023 Keysight Technologies, Inc. |