Extend Frequency Lock Range (TEDS)

Default: Selected (See Using Standard Setups/Presets)

Extend Frequency Lock Range, when selected, increases the frequency lock range by an additional +/-20kHz.

This is a control parameter for modulation analysis that allows an increase in the frequency lock range, within which you can analyze a TEDS signal by an additional +/-20kHz. Clear this check box only in special cases when specific data patterns are causing display instabilities.

See Also

Format Tab

Advanced Tab

Copyright © 2000-2023 Keysight Technologies, Inc.