Include Header Symbols (TEDS)

Default: Selected (See Using Standard Setups/Presets)

Header Symbols, when selected, configures the demodulator in the following manner:

Since header symbols are always coded in QPSK, they appear in the "corners" of constellation diagrams, regardless of the type of modulation. This means as data they appear as hex 0, 1, 2, or 3. If you clear the Header Symbols box, the Header symbols appear white (typical pilot color) on the constellation diagrams. If you select Header Symbols, the header symbols appear red (typical symbol color) on the constellation diagrams.

See Also

Slots and Symbols

TEDS Symbol Table

Format Tab

Analysis Tab

Advanced Tab

Copyright © 2000-2022 Keysight Technologies, Inc.