Using Standard Setups/Presets)
M-16QAM (except for Random Access: M-4QAM) (SeeQPSK), M-16QAM, M- 64QAM
M-4QAM (QAM used by the subcarriers in the TEDS signal being analyzed.
specifies the order ofThe three types of Multiple Quadrature Amplitude Modulation (MQAM) are described in the following topics: TEDS Demod Overview and Symbol Constellations. Further note that symbols patterns for Normal Downlink, Normal Uplink, and Control Uplink include Header Symbols that always transmit in M-4QAM, while the remainder of the data (except for sync and pilot) symbols transmit as a single modulation type. There are no Header symbols for Random Access Uplink using M-4QAM modulation.
TEDS is a format within the family of Multiple Quadrature Amplitude Modulation (MQAM) formats. MQAM are distinguished by multiple carriers of standard digital modulation, with each carrier called a subcarrier.
See Also
Copyright © 2000-2023 Keysight Technologies, Inc. |