Contiguous Slots (TEDS)

Default: 1

Range: 1 to number of slots possibly contained in Search Length

Contiguous Slots specifies how many slots are assumed to be contiguous in an uplink slot. This setting configures the RF envelope search algorithm to provide detection of the start of a series of contiguous slots.

The Contiguous Slots and Slot Offset parameters are only available when Slot Format is set to Control Uplink or Normal Uplink. For other slot formats, the Contiguous Slots and Slot Offset parameters are disabled and have no effect on analysis.

See Also

Slot Offset

Format Tab

TEDS Demod Properties Dialog Box

Copyright © 2000-2021 Keysight Technologies, Inc.