Slot Format (TEDS)

Default: See Using Standard Setups/Presets

Slot Format allows you to select one of the following TEDS slot formats:

Another method for selecting the slot format is to use the Preset to Standard button which prompts you to select a slot format. The Channel Bandwidth must be set prior to using the Preset to Standard button. Then Preset to Standard sets up the parameters for the selected channel bandwidth. (See Using Standard Setups/Presets.)

See Also

Slots and Symbols

Analysis Tab

Format Tab

Advanced Tab

ACP PvT Tab

Copyright © 2000-2021 Keysight Technologies, Inc.