Slot Offset (TEDS)

Default: 0

Range: 0 to Contiguous Slots - 1

Slot Offset specifies which slot within the set of contiguous active slots will be used for modulation analysis. Setting this value to zero implies the first slot of the set of contiguous slots will be analyzed.

The Contiguous Slots and Slot Offset parameters are only available when Slot Format is set to Control Uplink or Normal Uplink. For other slot formats, the Contiguous Slots and Slot Offset parameters are disabled and have no effect on analysis.

See Also

Contiguous Slots

Format Tab

TEDS Demod Properties Dialog Box

Copyright © 2000-2021 Keysight Technologies, Inc.