To display an Error Vector Time trace with Band Power Markers using a test signal for TEDS Normal Uplink, 50kHz, 16QAM:
Click within a trace, and then select
to view the composite Error Vector Time trace. To scale the trace, select .Configure Band Power markers
Click
In the
tab of the dialog, select the checkbox.Set
toMove the band power marker to the desired location by using the mouse to click and drag the marker or by setting the
and in the dialog. For example, Center = 15 sym and Span = 5 sym.Review the Band Power information at either the top of the trace (currently selected marker) or in the marker readout window.
See Also
Copyright © 2000-2023 Keysight Technologies, Inc. |