Click the
button to choose from the following preset standard formats:The Channel Bandwidth needs to be selected before the button is clicked. The preset parameters, including frequency span, ACP Offset, and ACP Bandwidth, are specific to the selected channel bandwidth (as well as the selected slot format).
Some parameters may need to be changed after a Preset to Standard, for example,
.After selecting Preset to Standard - Normal Uplink, the analyzer automatically enters the TEDS demodulation parameters appearing in the following table:
Parameter |
Channel Bandwidths |
|||
---|---|---|---|---|
25kHz BW |
50kHz BW |
100kHz BW |
150kHz BW |
|
.35 |
.35 |
.35 |
.35 |
|
18kHz |
18kHz |
18kHz |
18kHz |
|
25kHz |
37.5kHz |
62.5kHz |
87.5kHz |
|
-4 |
-4 |
-4 |
-4 |
|
1 |
1 |
1 |
1 |
|
selected |
selected |
selected |
selected |
|
.2 |
.2 |
.2 |
.2 |
|
75kHz |
100kHz |
150kHz |
200kHz |
|
cleared |
cleared |
cleared |
cleared |
|
selected |
selected |
selected |
selected |
|
selected |
selected |
selected |
selected |
|
selected |
selected |
selected |
selected |
|
cleared |
cleared |
cleared |
cleared |
|
16QAM |
16QAM |
16QAM |
16QAM |
|
selected |
selected |
selected |
selected |
|
55mSec |
55mSec |
55mSec |
55mSec |
|
0 |
0 |
0 |
0 |
|
1 |
1 |
1 |
1 |
After selecting Preset to Standard - Normal Downlink, the VSA automatically enters the TEDS demodulation parameters appearing in the following table:
|
Channel Bandwidths |
|||
---|---|---|---|---|
25kHz BW |
50kHz BW |
100kHz BW |
150kHz BW |
|
.35 |
.35 |
.35 |
.35 |
|
18kHz |
18kHz |
18kHz |
18kHz |
|
25kHz |
37.5kHz |
62.5kHz |
87.5kHz |
|
-4 |
-4 |
-4 |
-4 |
|
1 |
1 |
1 |
1 |
|
selected |
selected |
selected |
selected |
|
.2 |
.2 |
.2 |
.2 |
|
75kHz |
100kHz |
150kHz |
200kHz |
|
cleared |
cleared |
cleared |
cleared |
|
selected |
selected |
selected |
selected |
|
selected |
selected |
selected |
selected |
|
selected |
selected |
selected |
selected |
|
cleared |
cleared |
cleared |
cleared |
|
16QAM |
16QAM |
16QAM |
16QAM |
|
selected |
selected |
selected |
selected |
|
30mSec |
30mSec |
30mSec |
30mSec |
|
0 |
0 |
0 |
0 |
|
1 |
1 |
1 |
1 |
After selecting Preset to Standard - Random Access, the VSA automatically enters the TEDS demodulation parameters appearing in the following table:
Parameter |
Channel Bandwidth |
---|---|
25kHz BW |
|
.35 |
|
18kHz |
|
25kHz |
|
-4 |
|
1 |
|
selected |
|
.2 |
|
75kHz |
|
cleared |
|
selected |
|
selected |
|
selected |
|
cleared |
|
4QAM |
|
selected |
|
35mSec |
|
0 |
|
1 |
After selecting Preset to Standard - Control Uplink, the VSA automatically enters the TEDS demodulation parameters appearing in the following table:
|
Channel Bandwidths |
|||
---|---|---|---|---|
25kHz BW |
50kHz BW |
100kHz BW |
150kHz BW |
|
.35 |
.35 |
.35 |
.35 |
|
18kHz |
18kHz |
18kHz |
18kHz |
|
25kHz |
37.5kHz |
62.5kHz |
87.5kHz |
|
-4 |
-4 |
-4 |
-4 |
|
1 |
1 |
1 |
1 |
|
selected |
selected |
selected |
selected |
|
.2 |
.2 |
.2 |
.2 |
|
75kHz |
100kHz |
150kHz |
200kHz |
|
cleared |
cleared |
cleared |
cleared |
|
selected |
selected |
selected |
selected |
|
selected |
selected |
selected |
selected |
|
selected |
selected |
selected |
selected |
|
cleared |
cleared |
cleared |
cleared |
|
16QAM |
16QAM |
16QAM |
16QAM |
|
selected |
selected |
selected |
selected |
|
35mSec |
35mSec |
35mSec |
35mSec |
|
0 |
0 |
0 |
0 |
|
1 |
1 |
1 |
1 |
See Also
Selecting the TEDS Demodulator
Copyright © 2000-2023 Keysight Technologies, Inc. |