shows values that are applied to the acquired data to compensate for phase and magnitude anomalies in the measurement hardware and software signal processing, determined during calibration sequences. If a straight line, then there is no correction.
Select TEDS demod properties.
to scale the trace. If the trace shows NO DATA, check your recorded signal or hardware input andSee Also
Copyright © 2000-2023 Keysight Technologies, Inc. |