shows time-data before pulse search and demodulation, which is the acquired time data used to search for the pulse (or burst). The image below shows Normal Uplink, 50kHz channel bandwidth, 16QAM modulation signal
Select Search Length determines the maximum length of the trace. To change scales, see and choose from the format drop-down menu.
to scale the trace. The TEDS demod parameterSee Also
Copyright © 2000-2023 Keysight Technologies, Inc. |