Analysis Subcarrier. You can use this trace for comparison purposes with measured signals.
shows a sequence of ideal I and Q states for a specific
Select
to scale the trace. The trace shown above is the constellation trace for the reference signal (Normal Uplink, 50kHz channel bandwidth, 16QAM modulation).Select
to place a marker on the trace; then review the symbol information in the marker readout window. Once you have a marker on the trace, use your left and right arrow keyboard keys to move the marker through the symbols.To view this same trace as a measured composite signal, see Overlaid IQ Ref Time.
See Also
Copyright © 2000-2023 Keysight Technologies, Inc. |