This topic provides information on connecting and successfully demodulating a signal using the LTE demodulator. A typical measurement includes the following measurement setup process (each step is discussed in the following text).
Downlink parameters
Set the Result Length, Measurement Interval, and Measurement Offset
Set Mirrored Spectrum when necessary
Connect your Signal to the VSA
Single or multiple channel connection
Connect the antenna signals to the hardware input channels.
Click
and select the number of channels.Connect the I and Q signals to the measurement hardware. To configure the VSA, choose one of the I+jQ selections:
.Notes for I+jQ input:
Recall the recorded signal by selecting
The center frequency and input range will be set by the recording.
Information about sample LTE signals included with the 89600 VSA software can be found in the Demo and Recorded Signals topic.
For more information about your specific measurement hardware, see the Measurement Hardware book.
Configure Measurement Setup and Input Parameters
Set the Center Frequency
By default, the center frequency of each measurement channel must be set to within approximately ±0.5x subcarrier spacing (7.5 KHz at the default subcarrier spacing) of the carrier frequency of the LTE signal connected to that channel, otherwise the demodulator may not be able to lock onto your signal.
Frequency lock range can be extended to 2.5x subcarrier spacing by selecting Extended Freq Lock.
Set the Frequency Span (optional)
At this point, you can set the frequency span for the signal. The span should be larger than the bandwidth of the LTE signal, and, for best results, set the span according to the LTE standard.
This step is optional because clicking Preset to Standard (this is part of Step 3 below) will set the span according to the LTE standard for the selected bandwidth.
Configure the Input Range
The input range must be set correctly to obtain accurate measurements. Input ranges that are too low overload the measurement hardware's ADC. Input ranges that are too high increase noise, which increases errors reported in error summary data, such as EVM.
Set up triggering (optional)
The default triggering mode is set to "FreeRun." However, you can configure a different type of configuring if you wish (such as an external frame trigger).
Verify the input signal and initial parameter settings
View your signal in the frequency domain (Spectrum trace) to verify the parameters you set.
To configure the demodulator to use a E-UTRA Test Model, see Selecting LTE Test Models.
Click
to enable the LTE demodulator properties and measurement parameters.Set Duplex Mode to FDD or TDD
For TDD:
Set uplink-downlink configuration (UL/DL Config)
Set special subframe configuration (Dw/GP/Up Len)
Set Direction to uplink or downlink
Preset to Standard: choose bandwidth
Demodulator measurement parameters will be set to typical values (see Using a Standard Setup topic) when Preset to Standard is used to select an LTE bandwidth. In addition to setting the demodulator parameters, the sample rate (and measurement span) will be set according to the standard for the chosen bandwidth.
These parameters are not autodetected and will need to be set when the default values are not correct for your signal.
Downlink
Uplink
Set the Result Length, Measurement Interval, and Measurement Offset
determines the available analysis data in terms of the number of slots + symbols. Set to capture the desired data.
Analysis Start Boundary to the .
specifies the data that will be demodulated, and specifies an offset from the beginning of theSet Mirrored Spectrum when necessary
LTE demodulation provides a feature that lets you configure the demodulator to conjugate the complex time-domain waveform. This has the effect of flipping the spectrum around the VSA's center frequency.
Press the Restart () button to restart the measurement.
For help when your signal is not demodulating correctly, see the Troubleshooting topic.
See Also
Measurement Speed Considerations
About Opts BHD and BHE: LTE Modulation Analysis
Copyright © 2000-2023 Keysight Technologies, Inc. |