Measurement Offset (Custom OFDM)

Measurement Offset specifies the start position of the Measurement Interval with respect to first symbol within the Result Length. Measurement Interval is entered as an integer number of symbols. The sum of the Measurement Interval plus Measurement Offset must fit within the measurement Result Length.

Measurement Interval specifies the time length (in symbols) of data within the Result Length that is used for computing and displaying the trace data results. The Measurement Offset is used to position the start of the Measurement Interval beyond the start of the measurement burst. The Result Length and Result Length Selection properties determine the maximum time length (in symbols) that the Measurement Interval can be positioned, see figure below.

See Also

Time Tab

Custom OFDM Demodulation Properties Dialog Box