Available Features (Digital Demod)
The standard set of VSA features are applicable to Digital Demodulation
with some exceptions, including:
- Time gating is
not available.
- , , and traces are not available.
- Averaging is
available for Error Vector Spectrum, IQ Meas Spec, and IQ Ref Spec as follows:
- rms
(video) computes an average of each rms error
update in the table.
- rms
exponential is like rms (video) except that averaging continues past the
average count with an exponential weighting.
- peak hold/continuous
peak hold keeps track of the peak rms error of each update in the table.
- Average Types applicable
to the pre-demodulated spectrum trace data results:
- rms
(video)
- rms
exponential
- peak hold/continuous
peak hold
Time averaging is not applied to time data but is applied
to the rms error information in the symbol
table.
See Also
Available Trace
Data (Digital Demod)
About Digital
Demodulation (Opt AYA)
89600 VSA software
Standard Features
2024
Copyright © 2000-2023 Keysight Technologies, Inc. |
|