Menu Path:
QPSK and can be thought of dually as:
is similar to OffsetThe FSK traces).
demodulator behaves like the 89600 VSA OQPSK demodulator (IQ traces), instead of like the CPM demodulator (To automatically configure the VSA for measuring signals that conform to the IRIG 106-04 standard, on the SOQPSK-TG (IRIG 106-04). Note that the SOQPSK-TG preset sets the symbol rate to 5 MHz although the standard does not define a specific symbol rate.
tab, click and selectFor more information about SOQPSK-TG, see the following document: http://www.irig106.org/docs/106-05/chapter2.pdf
To automatically configure the VSA for measuring signals that conform to the SOQPSK-A or SOQPSK-B standards, on the SOQPSK-A or SOQPSK-B.
tab, click and selectWhen using
, note the following:See Also
SOQPSK-TG (IRIG 106-04) filter
Copyright © 2000-2023 Keysight Technologies, Inc. |