The
dialog box contains parameters that configure the VSA's digital demodulator.In the
menu, is grayed (unavailable) if the digital demodulator is not enabled. To enable the digital demodulator, click .The dialog box contains five tabs:
Format tab: selects the demodulation format, Symbol Rate, , and .
From here, also select a standard setup to automatically configure the VSA to demodulate a known signal. For example, selecting the NADC standard setup configures the VSA to demodulate an NADC signal.
See Also
Setting up Digital Demod Measurement
Troubleshooting (Digital Demod)
About Digital Demodulation (Option AYA)
Copyright © 2000-2023 Keysight Technologies, Inc. |