The
selection determines whether the time data used in a Vector measurement is complex data or real data.When RF measurement path and the Start frequency is set to 0 Hertz. In this case, the VSA performs measurements on real-valued time data (no complex component).
is selected, the measurement hardware's (digital or analog) local oscillator (LO) is removed from theVector measurements and when the measurement hardware for the selected input channel supports digitizing the input signal without an analog or digital LO in the path.
can only be changed to forFor other configurations,
is always .When
is selected, the VSA performs measurements on complex time data. To obtain complex data, the VSA enables the measurement hardware's (digital or analog) LO. For measurement hardware that does not have an LO (such as oscilloscopes), the VSA performs the downconversion with its own digital LO.Zoom If Span Change check box.
automatically changes to when the frequency is set to a non-zero value. This also happens when you change the . To stay in mode when changing the , clear theThe term "baseband" identifies a measurement that has real time-domain data. In
mode, the signal is analyzed from 0 Hz to the highest frequency of interest. The term "zoom" identifies a measurement that has complex time-domain data. In zoomed mode, the signal is analyzed within a specified bandwidth, centered on the frequency of interest. measurements can start at 0 Hz or other frequencies.The VSA performs zoomed measurements using a digital LO (local oscillator). In some cases, the digital LO is in hardware.
The measurement is "zoomed" when there is a (digital or analog) LO in the RF measurement path. In this case, the input signal is mixed with the LO, and the resulting time-domain data is complex--contains both a real and an imaginary component.
The measurement is "baseband" when there is no LO in the RF measurement path. In this case the input signal (after filtering) is sampled directly by the A/D converter, and the resulting time-domain data is real.
See Also
Copyright © 2000-2023 Keysight Technologies, Inc. |