The parameter determines the length of the main time record.
By default, the span and number of frequency points. If a value is entered for that exceeds what is allowed by the current and number of , the VSA sets to the maximum allowable value. To increase the maximum value of , reduce the and/or increase the number of .
is limited by the frequencyIt is recommend to use the Auto Frequency Points mode which provides the most flexibility in specifying a or for a given span and window type.
Time record length and resolution bandwidth are inversely proportional, as shown by the following formula. Changing the time record length changes ResBW and vice-versa.
where: |
Time Record Length = Main Time Length ResBW = Resolution bandwidth Also, see Equivalent Noise Bandwidth. |
When the time record length length is changed, the VSA automatically sets
to and to to allow:When time gating is on, is determined by gate length, not . In this case, changing gate length changes ResBW and vice-versa.
The maximum time record length is determined by the number of Frequency Points and the measurement's frequency Span (which determines the sample rate, which determines the time between samples).
The minimum time record length is determined by the maximum ResBW setting (0.3 * Span).
For a more in depth explanation of these relationships, see Understanding Time and Frequency parameters.
The time record length (T seconds) is limited by the number of
and the frequency .
where: FP = number of
This can be derived through the following steps:
TP (max) = a * (FP - 1)
T (max) = TP (max) * Dt = (a * (FP - 1)) / (a * span) = (FP - 1) / span
where
TP = number of points in time record
Dt = 1 / f
f = a * span
a = 1.28 (for zoom data, i.e. complex time samples)
a = 2.56 (for baseband data, i.e. real time samples)
Minimum time record length is dependent on the resolution bandwidth to span ratio:
The maximum resolution bandwidth allowed by the VSA is 0.3 * span.
For a given window type, the minimum resolution bandwidth, while not directly affected by
and number of , may be limited by these parameters.See Also
Copyright © 2000-2023 Keysight Technologies, Inc. |