Color Tab (Display Preferences)

The Color tab in the Display Preferences dialog sets the colors of user interface elements including traces, the marker readout window, symbol points, the grid, and trace background.

To change a color, select the item from the list, and click the Color... button. A standard Windows color selection dialog box opens that selects a standard color or to define a custom color for that user interface element.

Colors are saved in .dspx files. (From the File menu, select Save > Save Display Preferences).

Universal settings

These settings apply for all traces and cannot be set independently for each trace:

Trace-specific or measurement-specific settings

These settings affect only the specified trace: