0
0-8
LTE TDD signal. There are nine special subframe configurations for Normal CP length and seven special subframe configurations for Extended CP length. These configurations are listed in Table 4.2-1 in 3GPP TS 36.211.
specifies which special subframe configuration is being used in anThis parameter only applies to LTE Frame Type 2 TDD signals and is only present on the Format tab when Duplex Mode is set to .
See Also
LTE Demod Properties Dialog Box
Copyright © 2000-2023 Keysight Technologies, Inc. |