Menu Path:
The LTE signals.
dialog box contains parameters that let you configure the VSA to demodulateThe LTE demodulator must be selected before this dialog box is available. To enable the demodulator, click
The
dialog box contains tab headings that group similar configuration parameters as follows:Format Tab: Lets you access basic demod configuration parameters such as sync type, Cell ID, CP length, and number of antennas.
Profile Tab: Lets you choose which channels are shown on traces and used in calculations, such as EVM or Power, as well as specify user channel allocations and control channel parameters.
Time tab: Lets you specify what part of the signal to analyze.
Advanced tab: Lets you specify signal adjustment and correction parameters.
5G Candidate: Lets you configure demodulation parameters for 5G candidate signals over LTE.
See Also
Measurement Speed Considerations
Copyright © 2000-2023 Keysight Technologies, Inc. |