PBCH is the Physical Broadcast Channel and is present in downlink signals only. PBCH is transmitted on symbols 0, 1, 2, and 3 of slot 1 and occupies the center 72 subcarriers. PBCH is not transmitted on any resource elements assigned to C-RS for antenna ports 0, 1, 2, and 3.
The modulation type of PBCH is QPSK.
PBCH contains the MIB part of the MAC layer channel BCH. The other part of BCH (System Information Block) is contained in a PDSCH allocation encoded with the SI-RNTI.
See Also
Copyright © 2000-2023 Keysight Technologies, Inc. |