Menu Path:
tabThe RBW) and packet/symbol timing. These settings affect the time analysis provided to the Low | Mid | High Band Packet Time traces and the corresponding spectrum analysis provided to the Low | Mid | High Band Packet Spectrum, as well as the composite traces Packet Spectrum and Packet Time. Click on a parameter link for specific parameter information.
tab accesses packet setup parameters including (See Also
Advanced Tab (MB-OFDM Demod Properties)
Format Tab (MB-OFDM Demod Properties)
Time Tab (MB-OFDM Demod Properties)
Copyright © 2000-2023 Keysight Technologies, Inc. |