To start the 89600 VSA Software I/O Connections utility, click
. Then use the I/O Connections utility to add an instrument in any of the following ways.Click
on the toolbar.Right-click anywhere in the Explorer Pane, then select
.From the menu bar, click
.When the following
Dialog Box appears, select the hardware you wish to add and click .
The remaining steps necessary to add an instrument are done in the Add LAN Instrument I/O Connections Configurable Properties Dialog Box.
See Also
I/O Connections Configurable Properties Dialog Box
I/O Connections with Logic Analyzers Overview
Copyright © 2000-2023 Keysight Technologies, Inc. |