TheOFDM modulated signals.
dialog box contains parameters that configure the VSA to demodulate 802.11a/g/j/pThe
demodulator must be selected before this dialog box is available. To enable the demodulator, click .The dialog box contains these tabs:
Advanced Tab: Specifies advanced parameters used to demodulate nonstandard and/or user defined 802.11a/g/j/p OFDM signals and to manipulate trace data results.
Format Tab: Specifies the 802.11a/g/j/p OFDM configuration parameters. These are the parameters necessary for the VSA to lock on to and demodulate the test signal.
Time Tab: Specifies the signal capture configuration parameters. These parameters are used to select the pulse search length and to isolate a segment of the time record for further viewing and data analysis.
See Also
Selecting 802.11a/g/j/p OFDM Demodulator
Setting up an 802.11a/g/j/p OFDM Measurement
Copyright © 2000-2023 Keysight Technologies, Inc. |