IEEE 802.11a/g this includes symbol data for both the SIGNAL and DATA symbols.
Demodulation is enabled, selecting Syms/Errs trace data shows the symbol table. The symbol table shows the error summary data and the symbol data (binary bits) for each symbol-time and subcarrier following the preamble. ForThe lower section of the OFDM symbol following the preamble symbols in the data stream.
trace data display shows the raw data bits for each symbol and subcarrier following the preamble. These bits are not decoded and include bits for all subcarrier symbols including the pilot subcarriers. The first bit in the table corresponds to the first bit of subcarrier number -26 of the firstThe default symbol table display shows the Data subcarrier symbol bits in yellow, the Pilot subcarrier symbol bits in white, and all the subcarrier number 0 symbol bits are blanked (not shown).
When the symbol table marker is enabled, the marker highlights the data bits for the selected subcarrier symbol and the marker readout provides the subcarrier number, the symbol number, and its value in decimal.
For IEEE 802.11a/g signals, the subcarrier modulation format used for symbol 0 (the SIGNAL symbol data, which uses BPSK modulation,1 bit/sym) may be different than the modulation format used for subsequent symbols (the DATA symbol data). The symbol table can show only one modulation format at a time, so the SIGNAL symbol (symbol 0) is displayed with the same number of bits/symbol as the DATA symbols (symbols 1). The extra characters are only pad bits and do not effect measurement data results.
To make the table easier to read, the symbol data is shown in groupings of eight characters followed by a space. The characters can represent a binary digit or a hexadecimal digit as specified by the Symbol Table Format parameter. The number to the left of each row indicate either the bit or symbol offset position depending the symbol table format as described below:
The symbol data bit format is binary and each character represents a binary digit. The number to the left of each row indicates the bit offset of the first bit in the row.
The symbol data bit format is hexadecimal and each character represents a hexadecimal digit. The number to the left of each row indicate the subcarrier symbol offset of the first subcarrier symbol in the row.
There must be at least 4 bits/symbol to use the hexadecimal format--that is, symbols that have less than 4 bits/symbol are displayed only in binary format regardless of the Symbol Table Format setting.
The symbol data bits can be shown in either binary or hexadecimal format, see Symbol Table Format.
The Result Length mode and parameters determines the number of symbols shown in the table.
Here's an easy way to identify bits that correspond to a point in the constellation diagram; Display the constellation diagram in one grid and the symbol table in another. Then turn on the markers for both displays and enable marker coupling. When the marker is placed on a point in the constellation diagram, the VSA highlights the corresponding symbol bits in the symbol table.
Use the keyboard arrow keys or the mouse wheel to move the marker from one symbol to the next. Use the Marker Position - X and Z Position parameters to move to a specific symbol location.
The upper section of this display shows the Error Summary data for 802.11a/g/j/p OFDM Demodulation. See About Error Summary Data for information about OFDM Error Summary Data.
See Also
Available Error Summary Data (802.11a/g/j/p OFDM)
Copyright © 2000-2023 Keysight Technologies, Inc. |