Overview

 

The Phase Noise application measures the phase noise of a DUT's output signal within a specified offset frequency range.

In this topic:

See Also

Features and Requirements

Features

Starting Phase Noise Application

How to start Phase Noise

Using Hardkey/SoftTab/Softkey

Using a mouse

  1. On the analyzer, press Meas > Meas Class....

  2. Select Phase Noise, then click OK.

  3. In the Confirm Measurement Class Change dialog, click OK to proceed or Cancel to exit.

  4. The Phase Noise application is displayed (shown below).

  1. Click Instrument.

  2. Select Meas Class....

  3. Select Phase Noise, then click OK.

  4. In the Confirm Measurement Class Change dialog, click OK to proceed or Cancel to exit.

  5. The Phase Noise application is displayed (shown below).

Phase Noise Display

The Phase Noise application measures the power density of the noise sideband relative to the power of the carrier over a start/stop offset frequency. The offset frequency corresponds to the distance from the carrier frequency. The log-transformed phase noise is displayed in dBc/Hz.

 

The bottom of the display area shows the carrier frequency, carrier power, and the Phase Noise start and stop offset frequencies. The x-axis is the offset frequency range displayed on a logarithmic scale to allow viewing the full offset range.

If the sweep time is greater than 2 seconds, a sweep indicator is displayed at the bottom of the display area to provide sweep time percentage complete:

Noise tables showing Spurious, Integrated Noise, and Spot Noise data can be displayed below the trace area.