When the PXB's power is switched on, it automatically logs into MS Windows using the default user name and password. This gives anyone full access to the system. The following steps can be taken to increase security of your instrument:
Require users to logon when the instrument is turned on - Learn how to enable this feature.
Set up individual accounts on the instrument with varying levels of access - Learn how to Add or Change User Accounts and Passwords.
|
You can create as many user accounts as you like. The user name is not case sensitive. The password is case sensitive. |
The following user accounts already exist on the PXB:
Account |
User name |
Password |
Details |
Default User |
Instrument |
measure4u |
PXBs are shipped from the factory with this account. Agilent recommends that you change the password and, if desired, the user name. Although allowed by Windows, do not delete this account. |
Administrator |
Administrator |
agilent4u |
PXBs are shipped from the factory with an Administrator account. This account is created by Windows and cannot be deleted |
|
AgilentOnly |
only4agil |
PXBs are shipped from the factory with an Agilent account. This account
is created by |
Guest |
|
|
This account allows anyone to type in any name, without a password, and gain limited access to the PXB files. This account is created by Windows and cannot be deleted. It can be renamed. This account is turned off when the instrument is shipped. |
Minimize the PXB user interface.
On the Windows task bar, click Start, then click Run.
In the Run dialog box, type control userpasswords2, then click OK.
In the User Accounts
dialog box that appears, check the Users
must enter a user name and password to use this computer check box. To turn this function off, perform the same procedure,
but clear the check box. The account that is selected when the check box
is cleared is the account that is automatically logged on when the instrument
is turned on.
|
To restore the PXB user interface, click the PXB icon in the task bar at the bottom of the screen. |
You can set up instrument users by name and grant various levels of access. This is particularly important when the PXB is remotely controlled or accessed over a LAN.
You can designate a person as the administrator and then configure the
PXB to allow others to use it with reduced permissions. That is, other
people can be signed on to use the instrument but they will not have the
ability to perform all of the administrative functions that you can as
the administrator.
Although allowed by Windows, do not allow an Administrator account without a password. Internet viruses look for and exploit this condition. See Antivirus Protection for your Instrument. |
Minimize the PXB user interface.
On the Windows task bar, click Start, then click Control Panel.
From the category view of the Control Panel, click User Accounts.
Under Pick a Category, click User Accounts.
Under or pick a Control Panel icon, select User Accounts.
Select from the following tasks under Pick a task:
Change an account
Create a new account
Change the way users log on or off
Follow the prompts to change
or add a new account.