The Pulse Setup dialogs are available with S9x025A/B, S9x024B or M9485A-025.
Note: (M980xA/P50xxA) In addition to S9x025A, option 021 (pulse modulation hardware) is required in order to output a pulsed modulated source signal. Option 021 is useless without S9x025A. In the multi-module configuration, only the modules with option 021 enables the pulse modulation.
Note: (P502xA-402) Options 021 and 022 add the pulse modulation capability on ports 1/2 and ports 3/4, respectively. For example, the pulsed modulated signal is not available on ports 1 and 2 when option 021 is not installed.
Note: The M937xA/P937xA does not support this function.
Note: (P50xxB) No hardware option is required. Pulse modulation hardware is not available for P50xxB. S97024xB or S97025xB is required. S97024xB is a limited version in the pulse period .
Note: With the pulse measurement on, the receiver gain is fixed to “Low” although “Auto” is shown in the dialog box. Set "High" manually if the high gain is required.
External pulse generators can be used along with the VNA internal pulse generators. Learn more.
In this topic
If pulse signals are required for an external device, Y1731A I/O adapter is necessary.
How to start the Pulse Setup dialog |
|
Using Hardkey/SoftTab/Softkey |
Using a mouse |
|
|
Note: The M937xA does not support this function. The Basic controls allow simple pulse measurements using the default (Autoselect) settings in the Advanced section of the dialog. Several VNA measurement settings are controlled by the Pulse setup, such as sweep type, number of points, and so forth. Pulse MeasurementNote: (M980xA, P50xxA/B) Fast mode for pulse modulation in the data sheet can be set by the SENSe:SWEep:PULSe:SHAPe. Off - Source and Receivers are NOT pulsed Standard Pulse - With pulsed RF, the VNA can be configured to sweep in frequency, power sweep, and CW time.
Pulse Profile - Pulse profile measurements provides a time domain (CW frequency) view of the pulse envelope. Profiling is performed using a measurement technique that "walks" a narrow receiver "snapshot" across the width of the pulse. This is analogous to using a camera to take many small snapshots of a wide image, then piecing them together to form a single, panoramic view. (This function is available in standard class only.) Pulse Profile measurement using default settings and R1 receiver.
Pulse TimingPulse Width - Sets the width of the source pulse. See measurement timing to learn how to control the receiver width and delay. Pulse Period The time to make one complete pulse. Pulse Frequency (PRF) The reciprocal of Period (1/ Period). See Internal Pulse Generators to learn more. By default, these settings configure Pulse Gen 1 to drive Source Modulators 1 and 2. This can be changed from the Advanced Settings Pulse Generator Setup dialog. -------- Advanced Settings ----------The following settings allow maximum control of a Pulse measurement. PropertiesAutoselect pulse detection method - This function is not available. Only Wide band is available in M9485A, M980xA, M983xA, P50xxA/B. In Standard Pulse:
In Pulse Profile:
Autoselect IF Path Gain and Loss - For future use. Optimize Pulse Frequency - Automatically selects the Pulse Frequency and Pulse Period. (This function is not available) Autoselect Profile Sweep Time - In Pulse Profile mode, adjusts the default X-axis start time to zero and the stop time double the Pulse Width. This allows you to see one complete pulse. If unchecked, the Sweep Time will not be changed. To adjust the X-axis manually, click OK to close the dialog. Then press Sweep > Main, then change the Start Time and Stop Time. Sweep Time - Sets the time the analyzer takes to complete one sweep. Number of Points - Sets the number of data points for the measurement. IFBW - Select the IFBW for the measurement.
Measurement TimingPort n, Rcvr - Used as RF Source Modulation Drive.
The Primary Clock is controlled by the internal or external pulse generator and is the primary pulse clock. The Internal and External selections are not the same as the Trigger Source Internal and External selections found in the Pulse Trigger tab of the Trigger dialog. However, they are inter-related as follows:
Autoselect Width and Delay - When checked, for Wideband mode and Pulse Gen = Pulse Trigger, the default setting for the receiver is adjusted to approximately 75% of the source pulse width, with 20% delay. This leaves approximately 5% of the source pulse ON after acquisition is complete. Autoselect Pulse Generators - When checked:
Pulse Generators... Click to launch the Pulse Generators Setup dialog.
|
Note: The M937xA and P937xA does not support this function. Pulse MeasurementOff - Source and Receivers are NOT pulsed Standard Pulse - With pulsed RF, the VNA can be configured to sweep in frequency, power sweep, and CW time. Pulse TimingRF Pulse Width - Sets the width of the RF Source pulse. Pulse Period pulldown- Allows the selection of the following: Pulse Period - The time to make one complete pulse. Pulse Frequency - The reciprocal of Period (1/ Period). Pulse Duty Cycle - Pulse Width divided by the Pulse Period. Labels
Pulse DetailsGenerator - Pulse generator outputs in numerical order. Device - Indicates the device being controlled by the pulse generator output.
Width - RF Source pulse width. This setting is the same as Pulse Width under RF Pulse. Delay - If the Offset Pulses using ADC Delay check box is disabled, then the delays are the pulse delays relative to the trigger. If the Offset Pulses using ADC Delay check box is enabled, then the delays are defined for the pulses relative to each other. In this case, you can enter negative delays, and the delay from the trigger will be adjusted to correct for these values. Invert - Check to cause the pulse ON time to be active low and OFF be active high. Enable Check to enable individual pulse generators. Autoselect Receiver Timing - Computes the width to 80% of the RF Source Width and the delay will be 10% of the RF Source Width. With this setting selected, the Width and Delay columns in the table are grayed out. Offset Pulses using ADC Delay Check Box
Timing Example Assume Pulse1 is used to modulate the RF signal, all Pulse outputs are enabled, all are set to zero delay, and all are set to the same width. The first timing diagram below is with offset off and the second timing diagram is with offset on.
ButtonsPlot Pulse Timing - Accesses pulse timing display to evaluate the pulse timing setup. Right-click in the display area to access the following menu: Autoscale - Automatically scales the data to fit vertically within the display grid area. Display marker annotation - Select to display marker annotation in the top-right of the display. Show graticule - Select to display graticules. Add marker to: - Select to add a marker to a displayed pulse trace. When a selection is made, the mouse pointer changes to a "+". Click in the display area and the marker will appear. Drag the marker to the desired position. Each time this selection is made, a new marker will be added. Copy to Clipboard - Copies a bitmap of the trace control (Display) to the clipboard. It can then be pasted into any document that accepts bitmaps. Print... - Prints the displayed data. Scale properties... - Accesses the following dialog: Stimulus - Sets the Begin and End displayed on the X-axis in seconds. Response - Sets the Reference level in the center of the Y-axis and sets the scale per division. Pulse Generators - Accesses the Pulse Generators Setup dialog. See below. |
This dialog is available with Option S9x025A/B and S9x024B (pulse generators). To see this dialog, press Pulse Generators... on the Pulse Setup dialog. Pulse GeneratorsConfigure the Pulse Generators to be used for your measurement. The pulse 0 is for the receiver. The pulse 1 is for source and P1 output and pulse 2 to 4 are for P2 to P4 output signal, receptively. When configured, external pulse generators appear in this list. Learn more. Delay defines the delay between the pulse clock and when the receiver begins to make a measurement. Learn more.
Important: If D + W is greater than P, then undefined VNA behavior results. There is NO error message or warning. P-(D+W) >120 ns should be satisfied (M9485A) Invert Check to cause the pulse ON time to be active low and OFF be active high. Enable Check to enable individual pulse generators. Trigger Choose from: (When ONE of these is changed, they ALL change. The internal Pulse Generators can NOT be triggered individually).
Frequency - Set the pulse frequency of each generator.
Period - Set the period of each generator. Learn more about the Pulse Generators. Pulsed Sources(M980xA, M983xA, P50xxA) The pulsed source is available with pulse modulation hardware option (021 or 022). Check to enable the required internal source ports. Modulator Drive - Choose the pulse generator to modulate the specified source. Choose from CW (NO pulse), Pulse 1, 2, 3, 4, External, PXI_TRIG0 to 7. Offset PulsesOffset Pulses using ADC Delay Check Box
Offset Pulse Example Assume Pulse1 is used to modulate the RF signal, all Pulse outputs are enabled, all are set to zero delay, and all are set to the same width. The first timing diagram below is with offsets off and the second timing diagram is with offsets on.
Pulsed ReceiversSynchronize ADCs using Pulse Trigger - Check to enable triggering used to gate the ADC for wideband receiver measurements. This is the same as Pulse0 Enable. The Width can NOT be configured. Pulse4 Output Indicates - Check to use an oscilloscope connected to the pulse 4 to display when the ADC is making measurements. There are two selections: All ADC Activity - When selected, all ADC activity can be monitored, including ADC activity that may not be displayed on a trace. An example is background measurements that are used for receiver leveling, but are not actually displayed on a trace. Trace ADC Activity - When selected, Pulse4 will be active only during measurements that will be displayed on a trace. Pulse Trigger.. - Click to start the Pulse Trigger dialog. Trigger... - Accesses the Trigger dialog for setting up triggering. Learn more.
|
To see this dialog, press Pulse Trigger on the Pulse Generator Setup dialog or select Stimulus, then Trigger from the VNA Menu. Trigger SourceSelect Internal or External to provide sync capability for the internal pulse generators.
(M9485A) The PULSE SYNC IN pin provides a configurable trigger signal into the Pulse Generators. Only one set of pulses is emitted when edge triggering is used. The length of time that it takes to emit one set of pulses is the end time of the last enabled pulse (largest of width + delay of all the pulses P0-P4). Trigger Level/EdgeSets the edge of the trigger signal to which the internal pulse generators will respond when being externally triggered at the PulseSyncIn pin. The level selection is not available. Positive = rising edge; Negative = falling edge. Receiver synchronizationSynchronize ADCs using pulse trigger - Check to enable triggering used to gate the ADC for wideband receiver measurements. The Width can NOT be configured. ADC trigger delay - Set the amount of time to wait before triggering the ADC to begin acquisition.
|
Using External Pulse Generators
Setup the External Pulse Generator as an External Device.
To perform a calibration in pulse mode, first configure and apply the pulse parameters (PRF, Pulse Width, Delays, IF gating, and so forth) before calibrating the system. This will ensure the VNA is configured properly during the calibration and measurement.