Last Updated: June 19, 2009
This command returns results for the Error Vector Magnitude (EVM) measurement.
Queries the EVM measurement results. The returned results are dependant on the setting of [SENSe:]RADIo:STANdard[:SELect]:WLAN[?].
Query Range for DSSS: Returns the following comma-separated scalar results when the modulation type is DSSS, that is [SENSe:]RADIo:STANdard[:SELect]:WLAN[?] is set to either B or GDSSs:
Bit Rate: The observed bit rate for data portion of the burst: a floating number Bit Rate and Modulation Format Values for DSSS and OFDM
Burst Quality: This indicates whether or not the measurement was performed on a good (1.0) or bad (0.0) burst: a floating point of 0.0 or 1.0
Chip Clock Frequency Error: The measured symbol clock frequency error of the measured burst(s): a floating point expressed in parts per million
Frequency Error: a floating point in Hz
Gated Power: a floating point in dBm
Header Status: This is information about the PLCP header: a floating point of the following values
1: No SFD sync pattern was found in the preamble, so the header is not valid.
2: Invalid bits were found in the header, but the header was still usable.
3: The header failed the CRC check.
4: An erroneous phase shift was found between the PLCP preamble and the PLCP header.
5: A 1 Mbps barker modulated burst was found with a short preamble, which is invalid for 802.11b.
6: The status of the header is unknown.
7: Everything about the header appears correct.
8: More than one result was found during a measurement that captured more than one 11b burst.
IQ Offset: a floating point in dB
MAC Status: This is status information about the MAC frame constrained in the PSDU portion of the burst: a floating point of the following values
1: The status is unknown, typically because the burst is longer than the period that was measured.
2: The MAC Frame Checksum (FCS) failed.
3: The MAC Frame Checksum (FCS) passed.
4: More than one result was found during a measurement that captured more than one 11b burst.
Modulation Format: The observed modulation format for the data portion of the burst. a floating point Bit Rate and Modulation Format Values for DSSS and OFDM
Peak EVM measured over the first 1000 chips of the burst: a floating point in %
RMS EVM: a floating point in %
Query Range for OFDM: Returns the following comma-separated scalar results when the modulation type is OFDM, that is [SENSe:]RADIo:STANdard[:SELect]:WLAN[?] is set to either A or GOFDm:
Bit Rate: The observed bit rate for data portion of the burst: a floating number Bit Rate and Modulation Format Values for DSSS and OFDM
Burst Quality: This indicates whether or not the measurement was performed on a good (1.0) or bad (0.0) burst: a floating point of 0.0 or 1.0
Frequency Error: a floating point in Hz
Gated Power: a floating point in dBm
IQ Gain Imbalance: a floating point in dB
IQ Offset: a floating point in dB
IQ Quadrature Error (sometimes referred to as quadrature skew): a floating point in degrees
Modulation Format: The observed modulation format for the data portion of the burst: a floating point Bit Rate and Modulation Format Values for DSSS and OFDM
RMS EVM: a floating point in %
Symbol Clock Frequency Error: a floating point expressed in parts per million
Query Range for MIMO 802.11n: Returns the following comma-separated scalar results when the modulation type is MIMO 802.11n, that is [SENSe:]RADIo:STANdard[:SELect]:WLAN[?] is set to N. There are 3 sets of results that can be returned using FETCh:EVM{0:2}? If no number is specified the default is 1:
FETCh:EVM0?: an array of points as follows:
The number of HT-LTF fields found in the observed burst: a floating point
Length of the HT-DATA field found (in symbols): a floating point
Modulation format of the HT-DATA field found in the analyzed burst: a floating point as detailed in Modulation Format Values for MIMO 802.11n
Power of the HT-DATA field found in the analyzed burst: a floating point in dBm
Indicates whether an HT-DATA field was found in the analyzed burst: a floating point of 0.0 (false) or 1.0 (true)
Indicates whether an HT-LTF field was found in the analyzed burst: a floating point of 0.0 (false) or 1.0 (true)
Length of the HT-SIG field found in the analyzed burst in symbols
Modulation format of the HT-SIG field found in the analyzed burst
Power of the HT-SIG field found in the analyzed burst: a floating point in dBm
Indicates whether an HT-SIG field was found in the analyzed burst: a floating point of 0.0 (false) or 1.0 (true)
Status of the HT-SIG demodulation
Length of the HT-STF field found in the analyzed burst in symbols: a floating point
Modulation format of the HT-STF field found in the analyzed burst: a floating point as detailed in Modulation Format Values for MIMO 802.11n
Power of the HT-STF field found in the analyzed burst: a floating point in dBm
Indicates whether an HT-STF field was found in the analyzed burst: a floating point of 0.0 (false) or 1.0 (true)
Length of the L-DATA field found in the analyzed burst in symbols
Modulation format of the L-DATA field found in the analyzed burst
Power of the L-DATA field found in the analyzed burst: a floating point in dBm
Indicates whether an L-DATA field was found in the analyzed burst: a floating point of 0.0 (false) or 1.0 (true)
Length of the L-LTF field found in the analyzed burst in symbols
Modulation format of the L-LTF field found in the analyzed burst: a floating point as detailed in Modulation Format Values for MIMO 802.11n
Power of the L-LTF field found in the analyzed burst: a floating point in dBm
Indicates whether an L-LTF field was found in the analyzed burst: a floating point of 0.0 (false) or 1.0 (true)
Length of the L-SIG field found in the analyzed burst in symbols
Modulation format of the L-SIG field found in the analyzed burst: a floating point as detailed in Modulation Format Values for MIMO 802.11n
Power of the L-SIG field found in the analyzed burst: a floating point in dBm
Indicates whether an L-SIG field was found in the analyzed burst: a floating point of 0.0 (false) or 1.0 (true)
Length of the L-STF field found in the analyzed burst in symbols
Modulation format of the L-STF field found in the input signal: a floating point as detailed in Modulation Format Values for MIMO 802.11n
Power of the L-STF field found in the analyzed burst: a floating point in dBm
Indicates whether an L-STF field was found in the analyzed burst: a floating point of 0.0 (false) or 1.0 (true)
Number of bytes of data in the PSDU, as decoded from the HT-SIG
Length of the entire
burst in
symbols
In the analyzed signal if any HT-LTF fields are found the following
3 results are returned for each HT-LTF field.
Length of the HT-LTF field found in the analyzed burst in symbols
Modulation format of the HT-LTF field found in the analyzed burst
Power of the HT-LTF field found in the analyzed burst: a floating point in dBm
FETCh:EVM1? or not specified: an array of points as follows:
Results common to all streams/channels
Burst Quality: This indicates whether or not the measurement was performed on a good (1.0) or bad (0.0) burst: a floating point of 0.0 or 1.0
Frequency Error: a floating point in Hz
MCS of observed signal: a floating point
The number of spatial streams of data found: a floating point
The number of subcarriers detected in the analyzed signal: a floating point
Spectral Flatness Margin: a floating point in dB. Only available for a single channel demodulation.
IEEE 802.11 standard detected
Symbol clock timing error: a floating point in ppm
Total burst power of all measured channels: a floating point in dB
Worst condition number:
a floating point
Individual channel results
Power in burst for channel 1: a floating point in dB
Data EVM measurement result for channel 1: a floating point in %
IQ Gain Imbalance for channel 1: a floating point in dB
IQ Offset for channel 1: a floating point in dB
IQ Quadrature Error for channel 1 (sometimes referred to as quadrature skew): a floating point in degrees
Peak EVM for channel 1 measured over the first 1000 chips of the burst: a floating point in %
Pilot EVM measurement result for channel 1: a floating point in %
RMS EVM for channel 1: a floating point in %
The correlation coefficient obtained when synchronizing to the L-STF part of the OFDM pulse for channel 1
Port used for channel 1: a floating point
Power in burst for channel 2: a floating point in dB
Data EVM measurement result for channel 2: a floating point in %
IQ Gain Imbalance for channel 2: a floating point in dB
IQ Offset for channel 2: a floating point in dB
IQ Quadrature Error for channel 2 (sometimes referred to as quadrature skew): a floating point in degrees
Peak EVM for channel 2 measured over the first 1000 chips of the burst: a floating point in %
Pilot EVM measurement result for channel 2: a floating point in %
RMS EVM for channel 2: a floating point in %
The correlation coefficient obtained when synchronizing to the L-STF part of the OFDM pulse for channel 2
Port used for channel 2: a floating point
Power in burst for channel 3: a floating point in dB
Data EVM measurement result for channel 3: a floating point in %
IQ Gain Imbalance for channel 3: a floating point in dB
IQ Offset for channel 3: a floating point in dB
IQ Quadrature Error for channel 3 (sometimes referred to as quadrature skew): a floating point in degrees
Peak EVM for channel 3 measured over the first 1000 chips of the burst: a floating point in %
Pilot EVM measurement result for channel 3: a floating point in %
RMS EVM for channel 3: a floating point in %
The correlation coefficient obtained when synchronizing to the L-STF part of the OFDM pulse for channel 3
Port used for channel 3: a floating point
Power in burst for channel 4: a floating point in dB
Data EVM measurement result for channel 4: a floating point in %
IQ Gain Imbalance for channel 4: a floating point in dB
IQ Offset for channel 4: a floating point in dB
IQ Quadrature Error for channel 4 (sometimes referred to as quadrature skew): a floating point in degrees
Peak EVM for channel 4 measured over the first 1000 chips of the burst: a floating point in %
Pilot EVM measurement result for channel 4: a floating point in %
RMS EVM for channel 4: a floating point in %
The correlation coefficient obtained when synchronizing to the L-STF part of the OFDM pulse for channel 4
Port used for channel
4: a floating point
Individual Stream Results
RMS level of the "Common Pilot Error" minus one for stream 1. This represents how much pilot tracking was needed during demodulation: a floating point
Data EVM measurement result for stream 1: a floating point in %
Peak EVM measurement result for stream 1: a floating point in %
Pilot EVM measurement result for stream 1: a floating point in %
RMS EVM measurement result for stream 1: a floating point in %
RMS level of the "Common Pilot Error" minus one for stream 2. This represents how much pilot tracking was needed during demodulation: a floating point
Data EVM measurement result for stream 2: a floating point in %
Peak EVM measurement result for stream 2: a floating point in %
Pilot EVM measurement result for stream 2: a floating point in %
RMS EVM measurement result for stream 2: a floating point in %
RMS level of the "Common Pilot Error" minus one for stream 3. This represents how much pilot tracking was needed during demodulation: a floating point
Data EVM measurement result for stream 3: a floating point in %
Peak EVM measurement result for stream 3: a floating point in %
Pilot EVM measurement result for stream 3: a floating point in %
RMS EVM measurement result for stream 3: a floating point in %
RMS level of the "Common Pilot Error" minus one for stream 4. This represents how much pilot tracking was needed during demodulation: a floating point
Data EVM measurement result for stream 4: a floating point in %
Peak EVM measurement result for stream 4: a floating point in %
Pilot EVM measurement result for stream 4: a floating point in %
RMS EVM measurement result
for stream 4: a floating point in %
Cross Power Results
Normalized cross power result for channel 1 from stream 2: a floating point in dB (this result is identical to the following result)
Normalized cross power result for channel 1 from stream 2: a floating point in dB (this result is identical to the previous result)
Normalized cross power result for channel 1 from stream 3: a floating point in dB
Normalized cross power result for channel 1 from stream 4: a floating point in dB
Normalized cross power result for channel 2 from stream 1: a floating point in dB (this result is identical to the following result)
Normalized cross power result for channel 2 from stream 1: a floating point in dB (this result is identical to the previous result)
Normalized cross power result for channel 2 from stream 3: a floating point in dB
Normalized cross power result for channel 2 from stream 4: a floating point in dB
Normalized cross power result for channel 3 from stream 1: a floating point in dB
Normalized cross power result for channel 3 from stream 2: a floating point in dB
Normalized cross power result for channel 3 from stream 4: a floating point in dB
Normalized cross power result for channel 4 from stream 1: a floating point in dB
Normalized cross power result for channel 4 from stream 2: a floating point in dB
Normalized cross power result for channel 4 from stream 3: a floating point in dB
FETCh:EVM2?: Returns an array which contains the spectral
flatness measurement results, one per subcarrier. These are normalized
to the average value of the central subcarriers as described in the standard,
such that a value of 0.0 is the average.
The numbers of results returned define the number of subcarriers. The array
of subcarriers is arranged such that array element 0 represents the lowest-frequency
subcarrier (eg subcarrier -28 in a 57-subcarrier signal).
Spectral flatness is defined in section 6.1 of the EWC HT PHY Specification document (section number taken from revision 1.25, 23-Dec-2005).
In a 20MHz channel and in corresponding 20MHz transmission in a 40MHz channel, the average energy of the constellations in each of the spectral lines – 16 to –1 and +1 to +16 shall deviate no more than ± 2 dB from their average energy. The average energy of the constellations in each of the spectral lines – 28 to –17 and +17 to +28 will deviate no more than +2/–4 dB from the average energy of spectral lines –16 to –1 and +1 to +16.
In a 40 MHz transmission the average energy of the constellations in each of the spectral lines –42 to –2 and +2 to +42 shall deviate no more than ± 2 dB from their average energy. The average energy of the constellations in each of the spectral lines –43 to –58 and +43 to +58 shall deviate no more than +2/–4 dB from the average energy of spectral lines –42 to –2 and +2 to +42. The data for this test will be based on the channel estimate step.
Bit Rate and Modulation Format Values for DSSS and OFDM
Return Value |
Description |
1.0 |
OFDM, 6 Mbps |
2.0 |
OFDM, 9 Mbps |
3.0 |
OFDM, 12 Mbps |
4.0 |
OFDM, 18 Mbps |
5.0 |
OFDM, 24 Mbps |
6.0 |
OFDM, 36 Mbps |
7.0 |
OFDM, 48 Mbps |
8.0 |
OFDM, 54 Mbps |
9.0 |
DSSS, 1 Mbps |
10.0 |
DSSS, 2 Mbps |
11.0 |
DSSS, 5.5 Mbps |
12.0 |
DSSS, 11 Mbps |
13.0 |
DSSS, 22 Mbps |
14.0 |
DSSS, 33 Mbps |
15.0 |
Unknown data rate |
16.0 |
Varying data rate was seen during multi-acquisition measurement |
Modulation Format Values for MIMO 802.11n
Return Value |
Description |
1.0 |
BPSK |
2.0 |
QPSK |
3.0 |
QAM16 |
4.0 |
QAM64 |
5.0 |
PSK8 |
6.0 |
Barker1 |
7.0 |
Barker2 |
8.0 |
CCK5.5 |
9.0 |
CCK11 |
10.0 |
PBCC5.5 |
11.0 |
PBCC11 |
12.0 |
PBCC22 |
13.0 |
PBCC33 |
14.0 |
Unknown format |
15.0 |
Barker2 with short preamble |
16.0 |
CCK5.5 with short preamble |
17.0 |
CCK11 with short preamble |
18.0 |
PBCC5.5 with short preamble |
19.0 |
PBCC11 with short preamble |
20.0 |
PBCC22 with short preamble |
21.0 |
PBCC33 with short preamble |
22.0 |
Various |
23.0 |
QAM256 |
24.0 |
RBPSK |
25.0 |
Auto |
26.0 |
HT-SIG |
Test Set Requirements: N8300A Wireless Networking Test Set Version A.02 and above
Example:
FETCh:EVM?
Queries the EVM measurement results.