Last updated: December 4, 2008
BCH Parameters
(
F7
). The menu on the right now displays the BCH Parms.
Cell Band
(
F8
) and select the appropriate cell band from the popup menu. NOTE |
If you selected DCS, please see How to Configure Access Burst Power Control for DCS for configuration instructions for the DCS 1800 band.
Operating Mode
(
F1
) and select
Cell Off
from the popup menu. The configurable parameters for controlling access burst power are only available when the test set's operating mode is
Cell Off
.
Cell Info
(
F6
).
Cell Parameters
(
F2
).
MS TX Power Max CCH (GSM or GPRS)
and select it.
Cell Parameters
area of the Cell Info screen displays changes to match the power level you've specified.For example, If the Cell Band is set to PGSM, and you set the MS TX Power Max CCH (GSM) to level 7 (which corresponds to 29 dBm), the maximum power the mobile station is allowed to transmit on the contol channel is 29 dBm.
Close Menu
(
F6
) and then
Return
(
F6
).
Operating Mode
(
F1
) and select
Active Cell
from the popup menu.