Last updated: December 3, 2008
This command is not applicable to the GSM Test Application. | ||
GPRS TA |
This command is not applicable to the GPRS Test Application. |
|
EGPRS TA |
This command is not applicable to the EGPRS Test Application. |
|
GSM/GPRS LA |
This command sets/queries the PBCCH channel state for Neighbour Cell <n>, where <n> is any integer 1 to 32. The Packet Broadcast Control Channel (PBCCH) state must be enabled for this parameter to take effect. |
|
EGPRS LA | ||
Requirements | GSM/GPRS/ EGPRS LA | |
OUTPUT 714;"CALL:PBCCH ON" ! Enables the PBCCH channel. |
GSM TA | This command is not applicable to the GSM test application. | |
This command is not applicable to the GPRS test application. | ||
This command is not applicable to the EGPRS test application. | ||
This command sets/queries the ARFCN for Neighbour Cell <n>, where <n> is any integer 1 to 32. The Packet Broadcast Control Channel (PBCCH) state must be enabled for this parameter to take effect. |
||
See Default ARFCNs in PBCCH BA Table . | ||
Requirements | GSM/GPRS/ EGPRS LA | |
OUTPUT 714;"CALL:PBCCH:BA:TABLe:NCELl1:ARFCN?" ! Queries the ARFCN setting for Neighbour Cell 1. |
Function | GSM TA | This command is not applicable to the GSM test application. |
This command is not applicable to the GPRS test application. | ||
This command is not applicable to the GPRS test application. | ||
This command sets/queries the Base Station Color Code (BCC) for Neighbour Cell <n>, where <n> is any integer 1 to 32. The Packet Broadcast Control Channel (PBCCH) state must be enabled for this parameter to take effect. |
||
5 | ||
Requirements | GSM/GPRS/ EGPRS LA | |
OUTPUT 714;"CALL:PBCCH:BA:TABLe:NCELl1:BCCode 1" ! Sets the BCC for Neighbour Cell 1 of the selected cell band to 1. |
Function | GSM TA | This command is not applicable to the GSM test application. |
This command is not applicable to the GPRS test application. | ||
This command is not applicable to the GPRS test application. | ||
This command sets/queries the Network Color Code (NCC) for Neighbour Cell <n>, where <n> is any integer 1 to 32. The Packet Broadcast Control Channel (PBCCH) state must be enabled for this parameter to take effect. |
||
1 | ||
Requirements | GSM/GPRS/ EGPRS LA | |
OUTPUT 714;"CALL:PBCCH::BA:TABLe:NCELl1:NCCode 1" ! Sets the NCC for Neighbour Cell 1 of the selected cell band to 1. |
Function | GSM TA | This command is not applicable to the GSM test application. |
This command is not applicable to the GPRS test application. | ||
This command is not applicable to the GPRS test application. | ||
This command sets/queries the Routing Area Code (RAC) for Neighbour Cell <n>, where <n> is any integer 1 to 32. The Packet Broadcast Control Channel (PBCCH) state must be enabled for this parameter to take effect. |
||
1 | ||
Requirements | GSM/GPRS/ EGPRS LA | |
OUTPUT 714;"CALL:PBCCH:BA:TABLe:NCELl1:RACode 1" ! Sets the RAC for Neighbour Cell 1 of the selected cell band to 1. |
GSM TA | This command is not applicable to the GSM Test Application. | |
This command is not applicable to the GPRS Test Application. | ||
This command is not applicable to the EGPRS Test Application. | ||
GSM/GPRS LA |
This command sets/queries the Report Priority for Neighbour Cell <n>, where <n> is any integer 1 to 32. The Packet Broadcast Control Channel (PBCCH) state must be enabled for this parameter to take effect. |
|
Requirements | GSM/GPRS/ EGPRS LA | |
OUTPUT 714;"CALL:CELL:PBCCH:BA:TABLE:NCELL3:RPRIORITY HIGH" ! Sets Report Priority of Neighbour cell 3 to HIGH. |