This command is not applicable to GSM. | ||
This command is not applicable to the GSM/GPRS lab application. | ||
EGPRS LA |
Sets/queries the number of bits to test. This is the number of information bits to test. Information bits exclude stealing flags and midamble bits. Due to the burst structure, the number of bits actually tested can be larger. The actual number of bits tested is available as a measurement result. See FETCh:SBERror:COUNt? |
|
EGPRS TA | ||
Setting | ||
*RST Setting | ||
GSM/GPRS/ EGPRS TA |
||
GSM/GPRS/ EGPRS LA | ||
OUTPUT 714;"SETup:SBERror:COUNt 75000" ! Sets the number of bits to test to 75000. |
This command is not applicable to GSM. | ||
This command is not applicable to the GSM/GPRS lab application. | ||
EGPRS LA |
Sets/queries loopback delay control mode. If loopback delay control mode is automatic (Auto), the test set will determine the loopback delay value that will allow correlation between uplink information bits with downlink information bits. If loopback delay control mode is manual (not Auto), the test set will use the loopback delay value entered in the Loopback Delay field. Refer to. see SETup:SBERror:MANual:DELay Refer also to the ` Bit Error Measurement for a description of loopback delay and its use in the EGPRS SRB BER measurement. |
|
EGPRS TA | ||
Setting | ||
*RST Setting | ||
GSM/GPRS/ EGPRS TA |
||
GSM/GPRS/ EGPRS LA | ||
OUTPUT 714;"SETup:SBERror:LDControl:AUTO OFF" ! Sets SBER delay to manual the user must select the manual frame delay number. |
This command is not applicable to GSM. | ||
This command is not applicable to the GSM/GPRS lab application. | ||
EGPRS LA |
Sets/queries the number of bursts the test set will wait before correlating uplink bursts received with downlink bursts sent when loop delay control mode is manual (AUTO OFF). To set the delay mode to manual, refer to SETup:SBERror:LDControl:AUTO . This value is displayed in the Loopback Delay field when Auto is not displayed. (If you want to display this value and Auto is currently displayed, press the front-panel key labeled OFF ). Refer to ` Bit Error Measurement for a description of loopback delay and how it is used in this measurement. |
|
EGPRS TA | ||
Setting | ||
*RST Setting | ||
GSM/GPRS/ EGPRS TA |
||
GSM/GPRS/ EGPRS LA | ||
OUTPUT 714;"SETup:SBERror:MANual:DELay 4" ! Sets delay of 4 bursts. |