Last updated: December 2, 2008
A (PD)TCH can have one of eight midamble patterns. These patterns are called Training Sequence Codes (TSCs). The test set's BCC and Expected Burst parameters must be set to the TSC used by the mobile station in order for the test set to synchronize with the mobile station.
This parameter only applies when the Operating Mode is set to one of the Test Mode Operating Modes . The Expected Burst parameter allows you to configure the test set to decode a certain uplink midamble pattern (TSC0 through TSC7). Alternatively, selecting RACH for this parameter allows you to set the test set to expect the special midamble pattern used by a RACH burst. The Expected Burst TSC can be set with the CALL:BURSt:TYPE[:SELected] command. If the Expected Burst TSC is not set, the test set may not synchronize to the mobile station's input signal.
The BCC (Base Station Color Code) parameter allows you to configure the test set to generate a certain downlink TSC (0 through 7). The command to set this parameter is CALL[:CELL]:BCCode .
When the Operating Mode is set to one of the Test Mode Operating Modes or Active Cell Operating Mode , both the BCC (Base Station Color Code) and the Expected Burst must be set to the same TSC value on the test set that your mobile station uses. This ensures synchronization between the test set and the mobile station.
Operating Mode
is set to
Active Cell
(GSM, GPRS or EGPRS) if the Expected Burst matches the
BCC (Base Station Colour Code)
.See How Do I Set the Training Sequence Code (TSC)? for a detailed procedure on how to manually configure the uplink and downlink TSCs.
This section details how to set the Training Sequence Code (TSC). When the test set's operating mode is a test mode, you must set both the downlink and uplink TSC. The uplink TSC is set by following the Expected Burst Procedure , and the downlink TSC is set by following the BCC (Base Station Colour Code) Procedure parameter.
When the test set's operating mode is
Active Cell
, the test set utilizes the value that the
BCC (Base Station Colour Code)
parameter is set to for both the uplink and downlink TSC. That is, the mobile station transmits the uplink TSC to match the BCC setting.
This procedure details how to set the BCC (Base Station Colour Code) parameter. (This parameter is the same as the downlink TSC and the downlink midamble.)
Operating Mode
(
F1
), and use the knob to highlight and select
Cell Off.
Cell Info
(
F6
).
Cell Identification
(
F3
). Use the knob to highlight and select BCC (Base Station Colour Code). The value that you set the BCC parameter to is the downlink Training Sequence Code (TSC).
Close Menu
(
F6
).
Return
(
F6
) to go back to the
Call Setup Screen
.
Operating Mode
(
F1
), and use the knob to highlight and select an Active Cell Operating Mode or Test Mode Operating Mode.
Operating Mode
is set to
Active Cell
(GSM, GPRS or EGPRS) if the Expected Burst matches the
BCC (Base Station Colour Code)
.
Also, the default value for the BCC is 5. This setting for the BCC (or downlink TSC) must match the downlink TSC used by your mobile station.
This procedure is only applicable when the test set is in one of the Test Mode Operating Modes .
This procedure details how to set the Expected Burst parameter.The setting for this parameter is the setting for the uplink TSC. When the test set is in one of the test mode operating modes or active cell operating mode, the downlink TSC (see BCC (Base Station Colour Code) Procedure ) must match the uplink TSC.
Operating Mode
(
F1
), and use the knob to highlight and select one of the
Test Mode Operating Modes
(depending on your requirements)
.
Close Menu
(
F6
).