CALL:BCCHannel

Last updated: 2014-11-28

The settings below can be set in active cell operating mode only when the call status is Idle, or in other operating modes.

If BCCH Update Page is set to Auto and you change the settings while your UE is camped to the test set, the test set performs a Broadcast Channel (BCCH) Update Procedure ; If BCCH Update Page is set to Inhibit (the default value) and you change the settings while your UE is camped to the test set, the UE is informed to re-read the BCCH to observe the change (see CALL:BCCHannel:UPDAte:PAGE AUTO).

For more information on the GPIB Command conventions, see GPIB Command conventions

CALL[:CELL]:BCCHannel:N300

Function

Sets/queries the N300, which determines the maximum number of retransmissions of RRC Connection Request message.

Setting

Range: 0 to 7

Query

Range: 0 to 7

*RST Setting

0

Requirements

Test Application Revision: A.02.00 and above

Programming Example

"CALL:CELL:BCCHannel:N300 0"

CALL[:CELL]:BCCHannel:N312[:IDLE]

Function

Sets/queries the N312 Link Establishment In-Sync Count , which determines the number of “in-syncs” required when establishing DPCH and the connection status is idle.

Setting

Range: S1 | S2 | S4 | S10 | S20 | S50 | S100 | S200 | S400 | S600 | S800 | S1000

Query

same as setting

*RST Setting

S1

Requirements

Test Application Revision: A.02.00 and above

Programming Example

"CALL:BCCHannel:N312 S1"

CALL[:CELL]:BCCHannel:N312:CONNected

Function

Sets/queries the number of “in-syncs” required when establishing a dedicated channel when in the connection mode.

Setting

Range: S1 | S2 | S4 | S10 | S20 | S50 | S100 | S200 | S400 | S600 | S800 | S1000

Query

same as setting

*RST Setting

S1

Requirements

Test Application Revision: A.02.00 and above

Programming Example

"CALL:BCCHannel:N312:CONNected S1"

CALL[:CELL]:BCCHannel:N313

Function

Sets/queries the N313, which determines the maximum number of successive “out of sync” before starts T313.

Setting

Range: S1 | S2 | S4 | S10 | S20 | S50 | S100 | S200

Query

Range: S1 | S2 | S4 | S10 | S20 | S50 | S100 | S200

*RST Setting

S2

Requirements

Test Application Revision: A.02.00 and above

Programming Example

"CALL:BCCHannel:N313 S2"

CALL[:CELL]:BCCHannel:N315

Function

Sets/queries the N315, which specifies the maximum number of successive "in sync" received during T313 is activated.

Setting

Range: S1 | S2 | S4 | S10 | S20 | S50 | S100 | S200 | S400 | S600 | S800 | S1000

Query

Range: S1 | S2 | S4 | S10 | S20 | S50 | S100 | S200 | S400 | S600 | S800 | S1000

*RST Setting

S50

Requirements

Test Application Revision: A.02.00 and above

Programming Example

"CALL:BCCHannel:N315 S50"

CALL[:CELL]:BCCHannel:T300

Function

Sets/queries the T300, which determines how long UE will wait for RRC connection setup after sending RRC Connection Request message.

Setting

Range: MS400 | MS600 | MS800 | MS1000 | MS1200 | MS1400 | MS1600 | MS1800 | MS2000 | MS3000 | MS4000 | MS6000 | MS8000

Query

same as setting

*RST Setting

MS400

Requirements

Test Application Revision: A.02.00 and above

Programming Example

"CALL:CELL:BCCHannel:T300 MS400"

CALL[:CELL]:BCCHannel:T308

Function

Sets/queries the T308 timer.

Setting

Range: MS40 | MS80 | MS160 | MS320

Query

same as setting

*RST Setting

MS40

Requirements

Test Application Revision: A.03.00 and above

Programming Example

"CALL:BCCHannel:T308 MS40"

CALL[:CELL]:BCCHannel:T312[:IDLE]

Function

Sets/queries the T312, which determines how long UE will wait to get the N312 Link Establishment In-Sync Count (Idle) when establishing DPCH and the connection status is Idle.

Setting

Range: 1 to 15

Query

Range: 1 to 15

*RST Setting

1

Requirements

Test Application Revision: A.02.00 and above

Programming Example

"CALL:BCCHannel:T312 1"

CALL[:CELL]:BCCHannel:T312:CONNected

Function

Sets/queries the T312, which determines how long UE will wait to get the N312 Link Establishment In-Sync Count (Idle) when establishing DPCH in the connection mode.

Setting

Range: 1 to 15

Query

Range: 1 to 15

*RST Setting

1

Requirements

Test Application Revision: A.02.00 and above

Programming Example

"CALL:BCCHannel:T312:CONNected 1"

CALL[:CELL]:BCCHannel:T313

Function

Sets/queries the T313, which determines how long UE will wait to get N315 “in-syncs” after it detects N313 “out-of-sync”, before it triggers the radio link failure procedure.

Setting

Range: 0 to 15

Query

Range: 0 to 15

*RST Setting

3

Requirements

Test Application Revision: A.02.00 and above

Programming Example

"CALL:BCCHannel:T313 3"

CALL[:CELL]:BCCHannel:T3212

Function

Sets/queries the T3212 timer.

Setting

Range: 0 to 255 decihours

Query

Same as setting

*RST Setting

0

Requirements

Test Application Revision: A.03.00 and above

Programming Example

"CALL:BCCHannel:T3212 0"

CALL[:CELL]:BCCHannel:UPDate:PAGE

Function

Sets/queries the BCCH Update Page state. If it is set to Auto and you change the SIB settings while your UE is camped to the test set, the test set performs a Broadcast Channel (BCCH) Update Procedure (SIB Contents); If it is set to Inhibit (the default value) and you change the SIB settings while your UE is camped to the test set, the UE is informed to re-read the BCCH to observe the change. See Broadcast Channel (BCCH) Update Procedure (SIB Contents).

Setting

Range: AUTO | INHibit

Query

Range: AUTO | INH

*RST Setting

INH

Requirements

Test Application Revision: A.02.00 and above

Programming Example

"CALL:BCCHannel:UPDAte:PAGE INH"