How Do I Order and Retrieve UE Reported Measurement Results?

How Do I Order and Retrieve UE Reported Measurement Results?

Last updated: January 15, 2009

Lab Application - Cell 1/Cell 2 Measurements

  1. Establish a call between the test set and UE (see How Do I Set Up a Call and Make a Connection? )
  2. Select Handovers ( F5 ) from the Call Control 1 of 5 menu.
  3. Select Soft Handover Info ( F4 ).
  4. Turn Cell 2 Power ( F1 ) on if you would like to retrieve UE measurement results for cell 2 as well as cell 1.
  5. Press the More key under Soft Info to move to the 2 of 2 menu.
    • Set Report Measurement Type ( F2 ) and SFN-SFN OTD Measurement Type ( F4 ) to specify which measurements the UE should perform when Send Meas Request ( F5 ) is selected.
    • If you specified that the UE should measure DTCH BLER , set the BLER Rep Intrvl ( F1 ) as needed.
    • Select Send Meas Request ( F5 ) (this will only be present if you have a call connected). UE reported measurement results are displayed.

Lab Application - Compressed Mode Measurements (Inter Frequency and GSM Cells)

See How Do I Enable Compressed Mode and Obtain UE Measurement Results? .

Test Application - Cell 1 Measurements

  1. Establish a call between the test set and UE (see How Do I Set Up a Call and Make a Connection? )
  2. Press the left More key until you reach the Call Control 2 of 5 menu.
  3. Select UE Rep Meas ( F5 ).
  4. Set Report Measurement Type ( F2 ) to specify which measurements the UE should perform when Send Meas Request is selected.
  5. If you specified that the UE should measure DTCH BLER , set the BLER Rep Intrvl ( F1 ) as needed.
  6. Select Send Meas Request ( F5 ) (this will only be present if you have a call connected). UE reported measurement results are displayed.

Related Topics


UE Reported Measurements

How Do I Enable Compressed Mode and Obtain UE Measurement Results?