CALL:CONNected

CALL:CONNected

Last updated: October 19, 2012

GPIB Command Conventions

CALL:CONNected[:STATe]

Function

Queries the connected/disconnected state of the call. A one is returned if the call is in the connected state. A zero is returned if the call is in the idle (disconnected) state. If the call is in any state other than connected or idle, the query will hang until the call state transitions to the connected or idle state.

When used in conjunction with the CALL:CONNected:ARM and CALL:CONNected:TIMeout commands, the CALL:CONNected:STATe? command allows the control program to synchronize to call connection/disconnection. See Connected/Idle Query and Call State Change Detector .

Query

Range:   0|1

*RST Setting

0

Requirements

Test Application Revision: A.02 and above.

Lab Application Revision: A.01 and above

Programming Example

 
OUTPUT 714;"CALL:CONNECTED:STATE?"
! returns 1 if call is connected, 0 if call is idle.

CALL:CONNected:ARM[:IMMediate]

Function

Sets (arms) the call-state-change detector. Arming this detector allows the control program to tell the test set that it is expecting a change in the state of a call, prior to initiating the state change.

Once armed, the detector remains armed until there is a call state change to Idle or Connected from one of the transitory states, nor is it disarmed by any transitions from Idle to Idle or Connected to Connected.

When used in conjunction with the CALL CONNected:STATe? and the CALL:CONNected: TIMeout commands, the CALL:CONNected:ARM command allows the control program to synchronize with call processing state changes. See Call State Change Detector .

For an explanation of the :DONE?, :OPComplete?, :SEQuential, and :WAIT commands, s ee Call Processing Event Synchronization .

Requirements

Test Application Revision: A.02 and above.

Lab Application Revision: A.01 and above

Programming Example

 
OUTPUT 714;"CALL:CONNECTED:ARM:IMMEDIATE"
! Arms the call-state-change detector.

CALL:CONNected:ARM:STATe?

Function

Queries the arm state of the call-state-change detector. This command never hangs and immediately returns a one if the detector is armed, or a zero if the detector is not armed. See Call State Change Detector

Query

Range:   1|0

*RST Setting

0

Requirements

Test Application Revision: A.02 and above.

Lab Application Revision: A.01 and above

Programming Example

 
OUTPUT 714;"CALL:CONN:ARM:STATE?"
! Returns arm state of the call-state-change detector.

CALL:CONNected:CCPChannel:PRIMary[:SLEVel]

Function

The setting form of this command performs two functions: (1) sets the Cell 1 Connected P-CCPCH/SCH Level (see CALL:CONNected:CCPChannel:PRIMary:LEVel ) and (2) sets the Cell 1 Connected P-CCPCH/SCH state to on (see CALL:CONNected:CCPChannel:PRIMary:STATe ).

The query form of this command returns the Cell 1 Connected P-CCPCH/SCH Level .

See Connected DL Channel Levels .

Setting

Range: -20.00 dB to 0 dB

Resolution: 0.01

Query

Same as setting

*RST Setting

-5.35 dB (on)
Requirements

Test Application Revision: A.02 and above.

Lab Application Revision: A.01 and above

Programming Example

 
OUTPUT 714;"CALL:CONNected:CCPChannel:PRIMary -7"
! Sets P-CCPCH connected power offset to -7 dB and turns its state on.

CALL:CONNected:CCPChannel:PRIMary[:SLEVel]:HSDPa

Function

The setting form of this command performs two functions: (1) sets the HSDPA Cell 1 Connected P-CCPCH/SCH Level (see CALL:CONNected:CCPChannel:PRIMary:LEVel:HSDPa ) and (2) sets the HSDPA Cell 1 Connected P-CCPCH/SCH state to on (see CALL:CONNected:CCPChannel:PRIMary:STATe:HSDPa ).

The query form of this command returns the HSDPA Cell 1 Connected P-CCPCH/SCH Level .

See Connected DL Channel Levels .

Setting

Range: -20.00 dB to 0 dB

Resolution: 0.01

Query

Same as setting

*RST Setting

-12 dB (on)
Requirements

Test Application Revision: A.08.20 and above, with the required feature license.

Lab Application Revision: C.03 and above

Programming Example

 
OUTPUT 714;"CALL:CONNected:CCPChannel:PRIMary:HSDPa -7"
! Sets HSDPA P-CCPCH connected power offset to -7 dB and turns its state on.

CALL:CONNected:CCPChannel:PRIMary[:SLEVel]:HSPA

Function

The setting form of this command performs two functions: (1) sets the HSPA Cell 1 Connected P-CCPCH/SCH Level (see CALL:CONNected:CCPChannel:PRIMary:LEVel:HSPA ) and (2) sets the HSPA Cell 1 Connected P-CCPCH/SCH state to on (see CALL:CONNected:CCPChannel:PRIMary:STATe:HSPA ).

The query form of this command returns the HSPA Cell 1 Connected P-CCPCH/SCH Level .

See Connected DL Channel Levels .

Setting

Range: -20.00 dB to 0 dB

Resolution: 0.01

Query

Same as setting

*RST Setting

-12 dB (on)
Requirements

Test Application Revision: A.12 and above, with the required feature license.

Lab Application Revision: E.00.16 and above

Programming Example

 
OUTPUT 714;"CALL:CONNected:CCPChannel:PRIMary:HSPA -7"
! Sets HSPA P-CCPCH connected power offset to -7 dB and turns its state on.

CALL:CONNected:CCPChannel:PRIMary:LEVel

Function

Sets/queries the Cell 1 Connected P-CCPCH/SCH Level .

The Cell 1 Connected P-CCPCH/SCH Level can also be set using the CALL:CONNected:CCPChannel:PRIMary[:SLEVel] command.

See Connected DL Channel Levels .

Setting

Range: -20.00 dB to 0 dB

Resolution: 0.01

Query

Same as setting

*RST Setting

-5.35 dB
Requirements

Test Application Revision: A.02 and above.

Lab Application Revision: A.01 and above

Programming Example

 
OUTPUT 714;"CALL:CONNected:CCPChannel:PRIMary:LEVel -7"

CALL:CONNected:CCPChannel:PRIMary:LEVel:HSDPa

Function

Sets/queries the HSDPA Cell 1 Connected P-CCPCH/SCH Level .

The HSDPA Cell 1 Connected P-CCPCH/SCH Level can also be set using the CALL:CONNected:CCPChannel:PRIMary[:SLEVel]:HSDPa command.

See Connected DL Channel Levels .

Setting

Range: -20.00 dB to 0 dB

Resolution: 0.01

Query

Same as setting

*RST Setting

-12 dB
Requirements

Test Application Revision: A.08.20 and above, with the required feature license.

Lab Application Revision: C.03 and above

Programming Example

 
OUTPUT 714;"CALL:CONNected:CCPChannel:PRIMary:LEVel:HSDPa -7"

CALL:CONNected:CCPChannel:PRIMary:LEVel:HSPA

Function

Sets/queries the HSPA Cell 1 Connected P-CCPCH/SCH Level .

The HSPA Cell 1 Connected P-CCPCH/SCH Level can also be set using the CALL:CONNected:CCPChannel:PRIMary[:SLEVel]:HSPA command.

See Connected DL Channel Levels .

Setting

Range: -20.00 dB to 0 dB

Resolution: 0.01

Query

Same as setting

*RST Setting

-12 dB
Requirements

Test Application Revision A.12 and above, with the required feature license.

Lab Application Revision: E.00.16 and above.

Programming Example

 
OUTPUT 714;"CALL:CONNected:CCPChannel:PRIMary:LEVel:HSPA -7"

CALL:CONNected:CCPChannel:PRIMary:STATe

Function

Sets/queries the Cell 1 Connected P-CCPCH/SCH state.

The Cell 1 Connected P-CCPCH/SCH state can also be set using the CALL:CONNected:CCPChannel:PRIMary[:SLEVel] command.

See Connected DL Channel Levels .

Setting

Range: 1|ON|0|OFF

Query

Range: 1|0

*RST Setting

1 (on)
Requirements

Test Application Revision: A.02 and above.

Lab Application Revision: A.01 and above

Programming Example

 
OUTPUT 714;"CALL:CONNected:CCPChannel:PRIMary:STATe ON" 

CALL:CONNected:CCPChannel:PRIMary:STATe:HSDPa

Function

Sets/queries the HSDPA Cell 1 Connected P-CCPCH/SCH state.

The HSDPA Cell 1 Connected P-CCPCH/SCH state can also be set using the CALL:CONNected:CCPChannel:PRIMary[:SLEVel]:HSDPa command.

See Connected DL Channel Levels .

Setting

Range: 1|ON|0|OFF

Query

Range: 1|0

*RST Setting

1 (on)
Requirements

Test Application Revision: A.08.20 and above, with the required feature license.

Lab Application Revision: C.03 and above

Programming Example

 
OUTPUT 714;"CALL:CONNected:CCPChannel:PRIMary:STATe:HSDPa ON" 

CALL:CONNected:CCPChannel:PRIMary:STATe:HSPA

Function

Sets/queries the HSPA Cell 1 Connected P-CCPCH/SCH state.

The HSPA Cell 1 Connected P-CCPCH/SCH state can also be set using the CALL:CONNected:CCPChannel:PRIMary[:SLEVel]:HSPA command.

See Connected DL Channel Levels .

Setting

Range: 1|ON|0|OFF

Query

Range: 1|0

*RST Setting

1 (on)
Requirements

Test Application Revision A.12 and above, with the required feature license.

Lab Application Revision: E.00.16 and above.

Programming Example

 
OUTPUT 714;"CALL:CONNected:CCPChannel:PRIMary:STATe:HSPA ON" 

CALL:CONNected:CCPChannel:SECondary[:SLEVel]

Function

The setting form of this command performs two functions: (1) sets the Cell 1 Connected S-CCPCH Level (see CALL:CONNected:CCPChannel:SECondary:LEVel ) and (2) sets the Cell 1 Connected S-CCPCH state to on (see CALL:CONNected:CCPChannel:SECondary:STATe ).

The query form of this command returns the Cell 1 Connected S-CCPCH Level .

See Connected DL Channel Levels .

Setting

Range: -20.00 dB to 0 dB

Resolution: 0.01

Query

Same as setting

*RST Setting

-20.00 dB (off)
Requirements

Test Application Revision: A.02 and above.

Lab Application Revision: A.01 and above

Programming Example

 
OUTPUT 714;"CALL:CONNected:CCPChannel:SECondary -10"
! Sets S-CCPCH connected power offset to -10 dB and turns its state on.

CALL:CONNected:CCPChannel:SECondary[:SLEVel]:HSDPa

Function

The setting form of this command performs two functions: (1) sets the HSDPA Cell 1 Connected S-CCPCH Level (see CALL:CONNected:CCPChannel:SECondary:LEVel:HSDPa ) and (2) sets the HSDPA Cell 1 Connected S-CCPCH state to on (see CALL:CONNected:CCPChannel:SECondary:STATe:HSDPa ).

The query form of this command returns the HSDPA Cell 1 Connected S-CCPCH Level .

See Connected DL Channel Levels .

Setting

Range: -20.00 dB to 0 dB

Resolution: 0.01

Query

Same as setting

*RST Setting

-20.00 dB (off)
Requirements

Test Application Revision: A.08.20 and above, with the required feature license.

Lab Application Revision: C.03 and above

Programming Example

 
OUTPUT 714;"CALL:CONNected:CCPChannel:SECondary:HSDPa -10"
! Sets HSDPA S-CCPCH connected power offset to -10 dB and turns its state on.

CALL:CONNected:CCPChannel:SECondary[:SLEVel]:HSPA

Function

The setting form of this command performs two functions: (1) sets the HSPA Cell 1 Connected S-CCPCH Level (see CALL:CONNected:CCPChannel:SECondary:LEVel:HSPA ) and (2) sets the HSPA Cell 1 Connected S-CCPCH state to on (see CALL:CONNected:CCPChannel:SECondary:STATe:HSPA ).

The query form of this command returns the HSPA Cell 1 Connected S-CCPCH Level .

See Connected DL Channel Levels .

Setting

Range: -20.00 dB to 0 dB

Resolution: 0.01

Query

Same as setting

*RST Setting

-20.00 dB (off)
Requirements

Test Application Revision A.12 and above, with the required feature license.

Lab Application Revision: E.00.16 and above.

Programming Example

 
OUTPUT 714;"CALL:CONNected:CCPChannel:SECondary:HSPA -10"
! Sets HSPA S-CCPCH connected power offset to -10 dB and turns its state on.

CALL:CONNected:CCPChannel:SECondary:LEVel

Function

Sets/queries the Cell 1 Connected S-CCPCH Level .

The Cell 1 Connected S-CCPCH Level can also be set using the CALL:CONNected:CCPChannel:SECondary[:SLEVel] command.

See Connected DL Channel Levels .

Setting

Range: -20.00 dB to 0 dB

Resolution: 0.01

Query

Same as setting

*RST Setting

-20.00 dB
Requirements

Test Application Revision: A.02 and above.

Lab Application Revision: A.01 and above

Programming Example

 
OUTPUT 714;"CALL:CONNected:CCPChannel:SECondary:LEVel -5"

CALL:CONNected:CCPChannel:SECondary:LEVel:HSDPa

Function

Sets/queries the HSDPA Cell 1 Connected S-CCPCH Level .

The HSDPA Cell 1 Connected S-CCPCH Level can also be set using the CALL:CONNected:CCPChannel:SECondary[:SLEVel]:HSDPa command.

See Connected DL Channel Levels .

Setting

Range: -20.00 dB to 0 dB

Resolution: 0.01

Query

Same as setting

*RST Setting

-20.00 dB
Requirements

Test Application Revision: A.08.20 and above, with the required feature license.

Lab Application Revision: C.03 and above

Programming Example

 
OUTPUT 714;"CALL:CONNected:CCPChannel:SECondary:LEVel:HSDPa -5"

CALL:CONNected:CCPChannel:SECondary:LEVel:HSPA

Function

Sets/queries the HSPA Cell 1 Connected S-CCPCH Level .

The HSPA Cell 1 Connected S-CCPCH Level can also be set using the CALL:CONNected:CCPChannel:SECondary[:SLEVel]:HSPA command.

See Connected DL Channel Levels .

Setting

Range: -20.00 dB to 0 dB

Resolution: 0.01

Query

Same as setting

*RST Setting

-20.00 dB
Requirements

Test Application Revision A.12 and above, with the required feature license.

Lab Application Revision: E.00.16 and above.

Programming Example

 
OUTPUT 714;"CALL:CONNected:CCPChannel:SECondary:LEVel:HSPA -5"

CALL:CONNected:CCPChannel:SECondary:STATe

Function

Sets/queries the Cell 1 Connected S-CCPCH state.

The Cell 1 Connected S-CCPCH state can also be set using the CALL:CONNected:CCPChannel:SECondary[:SLEVel] command.

See Connected DL Channel Levels .

Setting

Range: 1|ON|0|OFF

Query

Range: 1|0

*RST Setting

0 (off)
Requirements

Test Application Revision: A.02 and above.

Lab Application Revision: A.01 and above

Programming Example

 
OUTPUT 714;"CALL:CONNected:CCPChannel:SECondary:STATe OFF" 

CALL:CONNected:CCPChannel:SECondary:STATe:HSDPa

Function

Sets/queries the HSDPA Cell 1 Connected S-CCPCH state.

The HSDPA Cell 1 Connected S-CCPCH state can also be set using the CALL:CONNected:CCPChannel:SECondary[:SLEVel]:HSDPa command.

See Connected DL Channel Levels .

Setting

Range: 1|ON|0|OFF

Query

Range: 1|0

*RST Setting

0 (off)
Requirements

Test Application Revision: A.08.20 and above, with the required feature license.

Lab Application Revision: C.03 and above

Programming Example

 
OUTPUT 714;"CALL:CONNected:CCPChannel:SECondary:STATe:HSDPa OFF" 

CALL:CONNected:CCPChannel:SECondary:STATe:HSPA

Function

Sets/queries the HSPA Cell 1 Connected S-CCPCH state.

The HSPA Cell 1 Connected S-CCPCH state can also be set using the CALL:CONNected:CCPChannel:SECondary[:SLEVel]:HSPA command.

See Connected DL Channel Levels .

Setting

Range: 1|ON|0|OFF

Query

Range: 1|0

*RST Setting

0 (off)
Requirements

Test Application Revision A.12 and above, with the required feature license.

Lab Application Revision: E.00.16 and above.

Programming Example

 
OUTPUT 714;"CALL:CONNected:CCPChannel:SECondary:STATe:HSPA OFF" 

CALL:CONNected:CPIChannel[:SLEVel]

Function

The setting form of this command performs two functions: (1) sets the Cell 1 Connected CPICH Level (see CALL:CONNected:CPIChannel:LEVel ) and (2) sets the Cell 1 Connected CPICH state to on (see CALL:CONNected:CPIChannel:STATe ).

The query form of this command returns the Cell 1 Connected CPICH Level .

See Connected DL Channel Levels .

Setting

Range: -20.00 dB to 0 dB

Resolution: 0.01

Query

Same as setting

*RST Setting

-3.30 dB (on)
Requirements

Test Application Revision: A.02 and above.

Lab Application Revision: A.01 and above

Programming Example

 
OUTPUT 714;"CALL:CONNected:CPIChannel -7"
! Sets CPICH connected power offset to -7 dB and turns its state on.

CALL:CONNected:CPIChannel[:SLEVel]:HSDPa

Function

The setting form of this command performs two functions: (1) sets the HSDPA Cell 1 Connected CPICH Level (see CALL:CONNected:CPIChannel:LEVel:HSDPa ) and (2) sets the HSDPA Cell 1 Connected CPICH state to on (see CALL:CONNected:CPIChannel:STATe:HSDPa ).

The query form of this command returns the HSDPA Cell 1 Connected CPICH Level .

See Connected DL Channel Levels .

Setting

Range: -20.00 dB to 0 dB

Resolution: 0.01

Query

Same as setting

*RST Setting

-10 dB (on)
Requirements

Test Application Revision: A.08.20 and above, with the required feature license.

Lab Application Revision: C.03 and above

Programming Example

 
OUTPUT 714;"CALL:CONNected:CPIChannel:HSDPa -7"
! Sets HSDPA CPICH connected power offset to -7 dB and turns its state on.

CALL:CONNected:CPIChannel[:SLEVel]:HSPA

Function

The setting form of this command performs two functions: (1) sets the HSPA Cell 1 Connected CPICH Level (see CALL:CONNected:CPIChannel:LEVel:HSPA ) and (2) sets the HSPA Cell 1 Connected CPICH state to on (see CALL:CONNected:CPIChannel:STATe:HSPA ).

The query form of this command returns the HSPA Cell 1 Connected CPICH Level .

See Connected DL Channel Levels .

Setting

Range: -20.00 dB to 0 dB

Resolution: 0.01

Query

Same as setting

*RST Setting

-10 dB (on)
Requirements

Test Application Revision: A.12 and above, with the required feature license.

Lab Application Revision: E.00.16 and above

Programming Example

 
OUTPUT 714;"CALL:CONNected:CPIChannel:HSPA -7"
! Sets HSPA CPICH connected power offset to -7 dB and turns its state on.

CALL:CONNected:CPIChannel:LEVel

Function

Sets/queries the Cell 1 Connected CPICH Level .

The Cell 1 Connected CPICH Level can also be set using the CALL:CONNected:CPIChannel[:SLEVel] command.

See Connected DL Channel Levels .

Setting

Range: -20.00 dB to 0 dB

Resolution: 0.01

Query

Same as setting

*RST Setting

-3.30 dB
Requirements

Test Application Revision: A.02 and above.

Lab Application Revision: A.01 and above

Programming Example

 
OUTPUT 714;"CALL:CONNected:CPIChannel:LEVel -7"

CALL:CONNected:CPIChannel:LEVel:HSDPa

Function

Sets/queries the HSDPA Cell 1 Connected CPICH Level .

The HSDPA Cell 1 Connected CPICH Level can also be set using the CALL:CONNected:CPIChannel[:SLEVel]:HSDPa command.

See Connected DL Channel Levels .

Setting

Range: -20.00 dB to 0 dB

Resolution: 0.01

Query

Same as setting

*RST Setting

-10 dB
Requirements

Test Application Revision: A.08.20 and above, with the required feature license.

Lab Application Revision: C.03 and above

Programming Example

 
OUTPUT 714;"CALL:CONNected:CPIChannel:LEVel:HSDPa -7"

CALL:CONNected:CPIChannel:LEVel:HSPA

Function

Sets/queries the HSPA Cell 1 Connected CPICH Level .

The HSPA Cell 1 Connected CPICH Level can also be set using the CALL:CONNected:CPIChannel[:SLEVel]:HSPA command.

See Connected DL Channel Levels .

Setting

Range: -20.00 dB to 0 dB

Resolution: 0.01

Query

Same as setting

*RST Setting

-10 dB
Requirements

Test Application Revision: A.12 and above, with the required feature license.

Lab Application Revision: E.00.16 and above

Programming Example

 
OUTPUT 714;"CALL:CONNected:CPIChannel:LEVel:HSPA -7"

CALL:CONNected:CPIChannel:STATe

Function

Sets/queries the Cell 1 Connected CPICH state.

The Cell 1 Connected CPICH state can also be set using the CALL:CONNected:CPIChannel[:SLEVel] command.

See Connected DL Channel Levels .

Setting

Range: 1|ON|0|OFF

Query

Range: 1|0

*RST Setting

1 (ON)
Requirements

Test Application Revision: A.02 and above.

Lab Application Revision: A.01 and above

Programming Example

 
OUTPUT 714;"CALL:CONNected:CPIChannel:STATe ON" 

CALL:CONNected:CPIChannel:STATe:HSDPa

Function

Sets/queries the HSDPA Cell 1 Connected CPICH state.

The HSDPA Cell 1 Connected CPICH state can also be set using the CALL:CONNected:CPIChannel[:SLEVel]:HSDPa command.

See Connected DL Channel Levels .

Setting

Range: 1|ON|0|OFF

Query

Range: 1|0

*RST Setting

1 (ON)
Requirements

Test Application Revision: A.08.20 and above, with the required feature license.

Lab Application Revision: C.03 and above

Programming Example

 
OUTPUT 714;"CALL:CONNected:CPIChannel:STATe:HSDPa ON" 

CALL:CONNected:CPIChannel:STATe:HSPA

Function

Sets/queries the HSPA Cell 1 Connected CPICH state.

The HSPA Cell 1 Connected CPICH state can also be set using the CALL:CONNected:CPIChannel[:SLEVel]:HSPA command.

See Connected DL Channel Levels .

Setting

Range: 1|ON|0|OFF

Query

Range: 1|0

*RST Setting

1 (ON)
Requirements

Test Application Revision: A.12 and above, with the required feature license.

Lab Application Revision: E.00.16 and above

Programming Example

 
OUTPUT 714;"CALL:CONNected:CPIChannel:STATe:HSPA ON" 

CALL:CONNected:DPCHannel[:SLEVel]

Function

The setting form of this command performs two functions: (1) sets the Cell 1 Connected DPCH Level (see CALL:CONNected:DPCHannel:LEVel ) and (2) sets the Cell 1 Connected DPCH state to on (see CALL:CONNected:DPCHannel:STATe ).

The query form of this command returns the Cell 1 Connected DPCH Level .

See Connected DL Channel Levels .

Setting

Range: -30.00 dB to 0 dB

Resolution: 0.01

Query

Same as setting

*RST Setting

-10.30 dB (on)
Requirements

Test Application Revision: A.02 and above.

Lab Application Revision: A.01 and above

Programming Example

 
OUTPUT 714;"CALL:CONNected:DPCHannel -7"
! Sets DPCH connected power offset to -7 dB and turns its state on.

CALL:CONNected:DPCHannel[:SLEVel]:HSDPa

Function

The setting form of this command performs two functions: (1) sets the HSDPA Cell 1 Connected DPCH Level (see CALL:CONNected:DPCHannel:LEVel:HSDPa ) and (2) sets the HSDPA Cell 1 Connected DPCH state to on (see CALL:CONNected:DPCHannel:STATe:HSDPa ).

The query form of this command returns the HSDPA Cell 1 Connected DPCH Level .

See Connected DL Channel Levels .

Setting

Range: -30.00 dB to 0 dB

Resolution: 0.01

Query

Same as setting

*RST Setting

-10 dB (on)
Requirements

Test Application Revision: A.08.20 and above, with the required feature license.

Lab Application Revision: C.03 and above

Programming Example

 
OUTPUT 714;"CALL:CONNected:DPCHannel:HSDPa -7"
! Sets HSDPA DPCH connected power offset to -7 dB and turns its state on.

CALL:CONNected:DPCHannel[:SLEVel]:HSPA

Function

The setting form of this command performs two functions: (1) sets the HSPA Cell 1 Connected DPCH Level (see CALL:CONNected:DPCHannel:LEVel:HSPA ) and (2) sets the HSPA Cell 1 Connected DPCH state to on (see CALL:CONNected:DPCHannel:STATe:HSPA ).

The query form of this command returns the HSPA Cell 1 Connected DPCH Level .

See Connected DL Channel Levels .

Setting

Range: -30.00 dB to 0 dB

Resolution: 0.01

Query

Same as setting

*RST Setting

-10 dB (on)
Requirements

Test Application Revision A.12 and above, with the required feature license.

Lab Application Revision: E.00.16 and above.

Programming Example

 
OUTPUT 714;"CALL:CONNected:DPCHannel:HSPA -7"
! Sets HSPA DPCH connected power offset to -7 dB and turns its state on.

CALL:CONNected:DPCHannel:LEVel

Function

Sets/queries the Cell 1 Connected DPCH Level .

The Cell 1 Connected DPCH Level can also be set using the CALL:CONNected:DPCHannel[:SLEVel] command.

See Connected DL Channel Levels .

Setting

Range: -30.00 dB to 0 dB

Resolution: 0.01

Query

Same as setting

*RST Setting

-10.30 dB
Requirements

Test Application Revision: A.02 and above.

Lab Application Revision: A.01 and above

Programming Example

 
OUTPUT 714;"CALL:CONNected:DPCHannel:LEVel -7"

CALL:CONNected:DPCHannel:LEVel:HSDPa

Function

Sets/queries the HSDPA Cell 1 Connected DPCH Level .

The HSDPA Cell 1 Connected DPCH Level can also be set using the CALL:CONNected:DPCHannel[:SLEVel]:HSDPa command.

See Connected DL Channel Levels .

Setting

Range: -30.00 dB to 0 dB

Resolution: 0.01

Query

Same as setting

*RST Setting

-10 dB
Requirements

Test Application Revision: A.08.20 and above, with the required feature license.

Lab Application Revision: C.03 and above

Programming Example

 
OUTPUT 714;"CALL:CONNected:DPCHannel:LEVel:HSDPa -7"

CALL:CONNected:DPCHannel:LEVel:HSPA

Function

Sets/queries the HSPA Cell 1 Connected DPCH Level .

The HSPA Cell 1 Connected DPCH Level can also be set using the CALL:CONNected:DPCHannel[:SLEVel]:HSPA command.

See Connected DL Channel Levels .

Setting

Range: -30.00 dB to 0 dB

Resolution: 0.01

Query

Same as setting

*RST Setting

-10 dB
Requirements

Test Application Revision A.12 and above, with the required feature license.

Lab Application Revision: E.00.16 and above.

Programming Example

 
OUTPUT 714;"CALL:CONNected:DPCHannel:LEVel:HSPA -7"

CALL:CONNected:DPCHannel:STATe

Function

Sets/queries the Cell 1 Connected DPCH state.

The Cell 1 Connected DPCH state can also be set using the CALL:CONNected:DPCHannel[:SLEVel] command.

See Connected DL Channel Levels .

Setting

Range: 1|ON|0|OFF

Query

Range: 1|0

*RST Setting

1 (on)
Requirements

Test Application Revision: A.02 and above.

Lab Application Revision: A.01 and above

Programming Example

 
OUTPUT 714;"CALL:CONNected:DPCHannel:STATe ON" 

CALL:CONNected:DPCHannel:STATe:HSDPa

Function

Sets/queries the HSDPA Cell 1 Connected DPCH state.

The HSDPA Cell 1 Connected DPCH state can also be set using the CALL:CONNected:DPCHannel[:SLEVel]:HSDPa command.

See Connected DL Channel Levels .

Setting

Range: 1|ON|0|OFF

Query

Range: 1|0

*RST Setting

1 (on)
Requirements

Test Application Revision: A.08.20 and above, with the required feature license.

Lab Application Revision: C.03 and above

Programming Example

 
OUTPUT 714;"CALL:CONNected:DPCHannel:STATe:HSDPa ON" 

CALL:CONNected:DPCHannel:STATe:HSPA

Function

Sets/queries the HSPA Cell 1 Connected DPCH state.

The HSPA Cell 1 Connected DPCH state can also be set using the CALL:CONNected:DPCHannel[:SLEVel]:HSPA command.

See Connected DL Channel Levels .

Setting

Range: 1|ON|0|OFF

Query

Range: 1|0

*RST Setting

1 (on)
Requirements

Test Application Revision A.12 and above, with the required feature license.

Lab Application Revision: E.00.16 and above.

Programming Example

 
OUTPUT 714;"CALL:CONNected:DPCHannel:STATe:HSPA ON" 

CALL:CONNected:DROP:TIMer[:STATe][:SELected]

Function

Sets/queries the call drop timer. The call drop timer indicates loss of uplink. This timer also determines when the demodulation of the uplink has been unsuccessful for a fixed period.

Setting

Range: 1|ON|0|OFF

Query

Range: 1|0

*RST Setting

1 (on)

Requirements

Test Application Revision: A.02 and above.

Lab Application Revision: A.01 and above

Programming Example

 
OUTPUT 714;"CALL:CONNECTED:DROP:TIMER:STATE 0"

CALL:CONNected:DROP:TIMer[:STATe]:WCDMa

Function

Sets/queries the call drop timer for the WCDMA format, whether or not that format is active. The call drop timer indicates loss of uplink. This timer also determines when the demodulation of the uplink has been unsuccessful for a fixed period.

Setting

Range: 1|ON|0|OFF

Query

Range: 1|0

*RST Setting

1 (on)

Requirements

Test Application Revision: A.02 and above.

Lab Application Revision: A.01 and above

Programming Example

 
OUTPUT 714;"CALL:CONNECTED:DROP:TIMER:STATE:WCDMA 0"

CALL:CONNected:EAGChannel[:SLEVel]

Function

The setting form of this command performs two functions: (1) sets the HSPA Cell 1 Connected E-AGCH Level (see CALL:CONNected:EAGChannel:LEVel ) and (2) sets the Cell 1 Connected E-AGCH state to on (see CALL:CONNected:EAGChannel:STATe ).

The query form of this command returns the HSPA Cell 1 Connected E-AGCH Level .

See Connected DL Channel Levels .

Setting

Range: -20.00 dB to 0 dB

Resolution: 0.01

Query

Same as setting

*RST Setting

-20 dB (on)

Requirements

Test Application Revision: A.12 and above, with the required feature license.

Lab Application Revision: E.00.16 and above

Programming Example

 
OUTPUT 714;"CALL:CONNected:EAGChannel -20"
! Sets the HSPA Cell 1 Connected E-AGCH Level
 to -20 dB and turns its state on.

CALL:CONNected:EAGChannel:LEVel

Function

Sets/queries the HSPA Cell 1 Connected E-AGCH Level .

The HSPA Cell 1 Connected E-AGCH Level can also be set using the CALL:CONNected:EAGChannel[:SLEVel] command.

See Connected DL Channel Levels .

Setting

Range: -20.00 dB to 0 dB

Resolution: 0.01

Query

Same as setting

*RST Setting

-20 dB

Requirements

Test Application Revision: A.12 and above, with the required feature license.

Lab Application Revision: E.00.16 and above

Programming Example

 
OUTPUT 714;"CALL:CONNected:EAGChannel:LEVel -20"

CALL:CONNected:EAGChannel:STATe

Function

Sets/queries the HSPA Cell 1 Connected E-AGCH Level state.

The HSPA Cell 1 Connected E-AGCH Level state can also be set using the CALL:CONNected:EAGChannel[:SLEVel] command.

See Connected DL Channel Levels .

Setting

Range: 1|ON|0|OFF

Query

Range: 1|0

*RST Setting

1 (on)

Requirements

Test Application Revision: A.12 and above, with the required feature license.

Lab Application Revision: E.00.16 and above

Programming Example

 
OUTPUT 714;"CALL:CONNected:EAGChannel:STATe ON" 

CALL:CONNected:EHIChannel[:SLEVel]

Function

The setting form of this command performs two functions: (1) sets the HSPA Cell 1 Connected E-HICH Level (see CALL:CONNected:EHIChannel:LEVel ) and (2) sets the HSPA Cell 1 Connected E-HICH Level state to on (see CALL:CONNected:EHIChannel:STATe ).

The query form of this command returns the HSPA Cell 1 Connected E-HICH Level .

See Connected DL Channel Levels .

Setting

Range: -20.00 dB to 0 dB

Resolution: 0.01

Query

Same as setting

*RST Setting

-20 dB (on)

Requirements

Test Application Revision: A.12 and above, with the required feature license.

Lab Application Revision: E.00.16 and above

Programming Example

 
OUTPUT 714;"CALL:CONNected:EHIChannel -20"
! Sets the HSPA Cell 1 Connected E-HICH Level
 to -20 dB and turns its state on.

CALL:CONNected:EHIChannel:LEVel

Function

Sets/queries the HSPA Cell 1 Connected E-HICH Level .

The HSPA Cell 1 Connected E-HICH Level can also be set using the CALL:CONNected:EHIChannel[:SLEVel] command.

See Connected DL Channel Levels .

Setting

Range: -20.00 dB to 0 dB

Resolution: 0.01

Query

Same as setting

*RST Setting

-20 dB

Requirements

Test Application Revision: A.12 and above, with the required feature license.

Lab Application Revision: E.00.16 and above

Programming Example

 
OUTPUT 714;"CALL:CONNected:EHIChannel:LEVel -20"

CALL:CONNected:EHIChannel:STATe

Function

Sets/queries the HSPA Cell 1 Connected E-HICH Level state.

The HSPA Cell 1 Connected E-HICH Level state can also be set using the CALL:CONNected:EHIChannel[:SLEVel] command.

See Connected DL Channel Levels .

Setting

Range: 1|ON|0|OFF

Query

Range: 1|0

*RST Setting

1 (on)

Requirements

Test Application Revision: A.12 and above, with the required feature license.

Lab Application Revision: E.00.16 and above

Programming Example

 
OUTPUT 714;"CALL:CONNected:EHIChannel:STATe ON" 

CALL:CONNected:ERGChannel[:SLEVel]

Function

The setting form of this command performs two functions: (1) sets the HSPA Cell 1 Connected E-RGCH Level (see CALL:CONNected:ERGChannel:LEVel ) and (2) sets the HSPA Cell 1 Connected E-RGCH Level state to on (see CALL:CONNected:ERGChannel:STATe ).

The query form of this command returns the HSPA Cell 1 Connected E-RGCH Level .

See Connected DL Channel Levels .

Setting

Range: -20.00 dB to 0 dB

Resolution: 0.01

Query

Same as setting

*RST Setting

-20 dB (off)

Requirements

Test Application Revision: A.12 and above, with the required feature license.

Lab Application Revision: E.00.16 and above

Programming Example

 
OUTPUT 714;"CALL:CONNected:ERGChannel -20"
! Sets the HSPA Cell 1 Connected E-RGCH Level
 to -20 dB and turns its state on.

CALL:CONNected:ERGChannel:LEVel

Function

Sets/queries the HSPA Cell 1 Connected E-RGCH Level .

The HSPA Cell 1 Connected E-RGCH Level can also be set using the CALL:CONNected:ERGChannel[:SLEVel] command.

See Connected DL Channel Levels .

Setting

Range: -20.00 dB to 0 dB

Resolution: 0.01

Query

Same as setting

*RST Setting

-20 dB

Requirements

Test Application Revision: A.12 and above, with the required feature license.

Lab Application Revision: E.00.16 and above

Programming Example

 
OUTPUT 714;"CALL:CONNected:ERGChannel:LEVel -20"

CALL:CONNected:ERGChannel:STATe

Function

Sets/queries the HSPA Cell 1 Connected E-RGCH Level state.

The HSPA Cell 1 Connected E-RGCH Level state can also be set using the CALL:CONNected:ERGChannel[:SLEVel] command.

See Connected DL Channel Levels .

Setting

Range: 1|ON|0|OFF

Query

Range: 1|0

*RST Setting

0 (off)

Requirements

Test Application Revision: A.12 and above, with the required feature license.

Lab Application Revision: E.00.16 and above

Programming Example

 
OUTPUT 714;"CALL:CONNected:ERGChannel:STATe OFF" 

CALL:CONNected:HSPDschannel[:SLEVel]

Function

The setting form of this command performs two functions: (1) sets the HSDPA Cell 1 Connected HS-PDSCHs Level (Sum) (see CALL:CONNected:HSPDschannel:LEVel ) and (2) sets the HSDPA Cell 1 Connected HS-PDSCHs Level (Sum) state to on (see CALL:CONNected:HSPDschannel:STATe ).

The query form of this command returns the HSDPA Cell 1 Sum of Active Conn HS-PDSCH Levels .

See Connected DL Channel Levels .

Setting

Range: -20.00 dB to 0 dB

Resolution: 0.01

Query

Same as setting

*RST Setting

-3 dB (on)

Requirements

Test Application Revision: A.08.20 and above, with the required feature license.

Lab Application Revision: C.03 and above

Programming Example

 
OUTPUT 714;"CALL:CONNected:HSPDschannel -4"
! Sets the Cell 1 Sum of Active Conn HS-PDSCH Levels
 to -4 dB and turns its state on.

CALL:CONNected:HSPDschannel[:SLEVel]:HSPA

Function

The setting form of this command performs two functions: (1) sets the HSPA Cell 1 Connected HS-PDSCHs Level (Sum) (see CALL:CONNected:HSPDschannel:LEVel:HSPA ) and (2) sets the HSPA Cell 1 Connected HS-PDSCHs Level (Sum) state to on (see CALL:CONNected:HSPDschannel:STATe:HSPA ).

The query form of this command returns the HSPA Cell 1 Sum of Active Conn HS-PDSCH Levels .

See Connected DL Channel Levels .

Setting

Range: -20.00 dB to 0 dB

Resolution: 0.01

Query

Same as setting

*RST Setting

-3 dB (on)

Requirements

Test Application Revision A.12 and above, with the required feature license.

Lab Application Revision: E.00.16 and above.

Programming Example

 
OUTPUT 714;"CALL:CONNected:HSPDschannel:HSPA -4"
! Sets the HSPA Cell 1 Sum of Active Conn HS-PDSCH Levels
 to -4 dB and turns its state on.

CALL:CONNected:HSPDschannel:LEVel

Function

Sets/queries the HSDPA Cell 1 Connected HS-PDSCHs Level (Sum) .

The HSDPA Cell 1 Connected HS-PDSCHs Level (Sum) can also be set using the CALL:CONNected:HSPDschannel[:SLEVel] command.

See Connected DL Channel Levels .

Setting

Range: -20.00 dB to 0 dB

Resolution: 0.01

Query

Same as setting

*RST Setting

-3 dB

Requirements

Test Application Revision: A.08.20 and above, with the required feature license.

Lab Application Revision: C.03 and above

Programming Example

 
OUTPUT 714;"CALL:CONNected:HSPDschannel:LEVel -4"

CALL:CONNected:HSPDschannel:LEVel:HSPA

Function

Sets/queries the HSPA Cell 1 Connected HS-PDSCHs Level (Sum).

The HSPA Cell 1 Connected HS-PDSCHs Level (Sum) can also be set using the CALL:CONNected:HSPDschannel[:SLEVel]:HSPA command.

See Connected DL Channel Levels .

Setting

Range: -20.00 dB to 0 dB

Resolution: 0.01

Query

Same as setting

*RST Setting

-3 dB

Requirements

Test Application Revision A.12 and above, with the required feature license.

Lab Application Revision: E.00.16 and above.

Programming Example

 
OUTPUT 714;"CALL:CONNected:HSPDschannel:LEVel:HSPA -4"

CALL:CONNected:HSPDschannel:STATe

Function

Sets/queries the HSDPA Cell 1 Connected HS-PDSCHs Level (Sum) state.

The HSDPA Cell 1 Connected HS-PDSCHs Level (Sum) state can also be set using the CALL:CONNected:HSPDschannel[:SLEVel] command.

See Connected DL Channel Levels .

Setting

Range: 1|ON|0|OFF

Query

Range: 1|0

*RST Setting

1 (on)

Requirements

Test Application Revision: A.08.20 and above, with the required feature license.

Lab Application Revision: C.03 and above

Programming Example

 
OUTPUT 714;"CALL:CONNected:HSPDschannel:STATe ON" 

CALL:CONNected:HSPDschannel:STATe:HSPA

Function

Sets/queries the HSPA Cell 1 Connected HS-PDSCHs Level (Sum) state.

The HSPA Cell 1 Connected HS-PDSCHs Level (Sum) state can also be set using the CALL:CONNected:HSPDschannel[:SLEVel]:HSPA command.

See Connected DL Channel Levels .

Setting

Range: 1|ON|0|OFF

Query

Range: 1|0

*RST Setting

1 (on)

Requirements

Test Application Revision A.12 and above, with the required feature license.

Lab Application Revision: E.00.16 and above.

Programming Example

 
OUTPUT 714;"CALL:CONNected:HSPDschannel:STATe:HSPA ON" 

CALL:CONNected:HSSCchannel[1][:SLEVel]

Function

The setting form of this command performs two functions: (1) sets the HSDPA Cell 1 Connected HS-SCCH 1 Level (see CALL:CONNected:HSSCchannel[1]:LEVel ) and (2) sets the HSDPA Cell 1 Connected HS-SCCH 1 Level state to on (see CALL:CONNected:HSSCchannel[1]:STATe ).

The query form of this command returns the HSDPA Cell 1 Connected HS-SCCH 1 Level .

See Connected DL Channel Levels .

Setting

Range: -20.00 dB to 0 dB

Resolution: 0.01

Query

Same as setting

*RST Setting

-10 dB (on)

Requirements

Test Application Revision: A.08.20 and above, with the required feature license.

Lab Application Revision: C.03 and above

Programming Example

 
OUTPUT 714;"CALL:CONNected:HSSCchannel -11"
! Sets the Cell 1 Connected HS-SCCH 1 Level

 to -11 dB and turns its state on.

CALL:CONNected:HSSCchannel[1][:SLEVel]:HSPA

Function

The setting form of this command performs two functions: (1) sets the HSPA Cell 1 Connected HS-SCCH 1 Level (see CALL:CONNected:HSSCchannel[1]:LEVel:HSPA ) and (2) sets the HSPA Cell 1 Connected HS-SCCH 1 Level state to on (see CALL:CONNected:HSSCchannel[1]:STATe:HSPA ).

The query form of this command returns the HSPA Cell 1 Connected HS-SCCH 1 Level .

See Connected DL Channel Levels .

Setting

Range: -20.00 dB to 0 dB

Resolution: 0.01

Query

Same as setting

*RST Setting

-10 dB (on)

Requirements

Test Application Revision A.12 and above, with the required feature license.

Lab Application Revision: E.00.16 and above.

Programming Example

 
OUTPUT 714;"CALL:CONNected:HSSCchannel:HSPA -11"
! Sets the HSPA Cell 1 Connected HS-SCCH 1 Level

 to -11 dB and turns its state on.

CALL:CONNected:HSSCchannel[1]:LEVel

Function

Sets/queries the HSDPA Cell 1 Connected HS-SCCH 1 Level .

The HSDPA Cell 1 Connected HS-SCCH 1 Level can also be set using the CALL:CONNected:HSSCchannel[1][:SLEVel] command.

See Connected DL Channel Levels .

Setting

Range: -20.00 dB to 0 dB

Resolution: 0.01

Query

Same as setting

*RST Setting

-10 dB

Requirements

Test Application Revision: A.08.20 and above, with the required feature license.

Lab Application Revision: C.03 and above

Programming Example

 
OUTPUT 714;"CALL:CONNected:HSSCchannel:LEVel -11"

CALL:CONNected:HSSCchannel[1]:LEVel:HSPA

Function

Sets/queries the HSPA Cell 1 Connected HS-SCCH 1 Level .

The HSPA Cell 1 Connected HS-SCCH 1 Level can also be set using the CALL:CONNected:HSSCchannel[1][:SLEVel]:HSPA command.

See Connected DL Channel Levels .

Setting

Range: -20.00 dB to 0 dB

Resolution: 0.01

Query

Same as setting

*RST Setting

-10 dB

Requirements

Test Application Revision A.12 and above, with the required feature license.

Lab Application Revision: E.00.16 and above.

Programming Example

 
OUTPUT 714;"CALL:CONNected:HSSCchannel:LEVel:HSPA -11"

CALL:CONNected:HSSCchannel[1]:STATe

Function

Sets/queries the HSDPA Cell 1 Connected HS-SCCH 1 Level state.

The HSDPA Cell 1 Connected HS-SCCH 1 Level state can also be set using the CALL:CONNected:HSSCchannel[1][:SLEVel] command.

See Connected DL Channel Levels .

Setting

Range: 1|ON|0|OFF

Query

Range: 1|0

*RST Setting

1 (on)

Requirements

Test Application Revision: A.08.20 and above, with the required feature license.

Lab Application Revision: C.03 and above

Programming Example

 
OUTPUT 714;"CALL:CONNected:HSSCchannel:STATe ON" 

CALL:CONNected:HSSCchannel[1]:STATe:HSPA

Function

Sets/queries the HSPA Cell 1 Connected HS-SCCH 1 Level state.

The HSPA Cell 1 Connected HS-SCCH 1 Level state can also be set using the CALL:CONNected:HSSCchannel[1][:SLEVel] command.

See Connected DL Channel Levels .

Setting

Range: 1|ON|0|OFF

Query

Range: 1|0

*RST Setting

1 (on)

Requirements

Test Application Revision A.12 and above, with the required feature license.

Lab Application Revision: E.00.16 and above.

Programming Example

 
OUTPUT 714;"CALL:CONNected:HSSCchannel:STATe:HSPA ON" 

CALL:CONNected:HSSCchannel2[:SLEVel]

Function

The setting form of this command performs two functions: (1) sets the HSDPA Cell 1 Connected HS-SCCH 2 Level (see CALL:CONNected:HSSCchannel2:LEVel ) and (2) sets the HSDPA Cell 1 Connected HS-SCCH 2 Level state to on (see CALL:CONNected:HSSCchannel2:STATe ).

The query form of this command returns the HSDPA Cell 1 Connected HS-SCCH 2 Level .

See Connected DL Channel Levels .

Setting

Range: -20.00 dB to 0 dB

Resolution: 0.01

Query

Same as setting

*RST Setting

-15 dB (off)

Requirements

Test Application Revision: A.08.20 and above, with the required feature license.

Lab Application Revision: C.03 and above

Programming Example

 
OUTPUT 714;"CALL:CONNected:HSSCchannel2 -11"
! Sets the Cell 1 Connected HS-SCCH 2 Level

 to -11 dB and turns its state on.

CALL:CONNected:HSSCchannel2[:SLEVel]:HSPA

Function

The setting form of this command performs two functions: (1) sets the HSPA Cell 1 Connected HS-SCCH 2 Level (see CALL:CONNected:HSSCchannel2:LEVel:HSPA ) and (2) sets the HSPA Cell 1 Connected HS-SCCH 2 Level state to on (see CALL:CONNected:HSSCchannel2:STATe:HSPA ).

The query form of this command returns the HSPA Cell 1 Connected HS-SCCH 2 Level .

See Connected DL Channel Levels .

Setting

Range: -20.00 dB to 0 dB

Resolution: 0.01

Query

Same as setting

*RST Setting

-15 dB (off)

Requirements

Test Application Revision A.12 and above, with the required feature license.

Lab Application Revision: E.00.16 and above.

Programming Example

 
OUTPUT 714;"CALL:CONNected:HSSCchannel2:HSPA -11"
! Sets the HSPA Cell 1 Connected HS-SCCH 2 Level

 to -11 dB and turns its state on.

CALL:CONNected:HSSCchannel2:LEVel

Function

Sets/queries the HSDPA Cell 1 Connected HS-SCCH 2 Level .

The HSDPA Cell 1 Connected HS-SCCH 2 Level can also be set using the CALL:CONNected:HSSCchannel2[:SLEVel] command.

See Connected DL Channel Levels .

Setting

Range: -20.00 dB to 0 dB

Resolution: 0.01

Query

Same as setting

*RST Setting

-15 dB

Requirements

Test Application Revision: A.08.20 and above, with the required feature license.

Lab Application Revision: C.03 and above

Programming Example

 
OUTPUT 714;"CALL:CONNected:HSSCchannel2:LEVel -11"

CALL:CONNected:HSSCchannel2:LEVel:HSPA

Function

Sets/queries the HSPA Cell 1 Connected HS-SCCH 2 Level .

The HSPA Cell 1 Connected HS-SCCH 2 Level can also be set using the CALL:CONNected:HSSCchannel2[:SLEVel]:HSPA command.

See Connected DL Channel Levels .

Setting

Range: -20.00 dB to 0 dB

Resolution: 0.01

Query

Same as setting

*RST Setting

-15 dB

Requirements

Test Application Revision A.12 and above, with the required feature license.

Lab Application Revision: E.00.16 and above.

Programming Example

 
OUTPUT 714;"CALL:CONNected:HSSCchannel2:LEVel:HSPA -11"

CALL:CONNected:HSSCchannel2:STATe

Function

Sets/queries the HSDPA Cell 1 Connected HS-SCCH 2 Level state.

The HSDPA Cell 1 Connected HS-SCCH 2 Level state can also be set using the CALL:CONNected:HSSCchannel2[:SLEVel] command.

See Connected DL Channel Levels .

Setting

Range: 1|ON|0|OFF

Query

Range: 1|0

*RST Setting

0 (off)

Requirements

Test Application Revision: A.08.20 and above, with the required feature license.

Lab Application Revision: C.03 and above

Programming Example

 
OUTPUT 714;"CALL:CONNected:HSSCchannel2:STATe ON" 

CALL:CONNected:HSSCchannel2:STATe:HSPA

Function

Sets/queries the HSPA Cell 1 Connected HS-SCCH 2 Level state.

The HSPA Cell 1 Connected HS-SCCH 2 Level state can also be set using the CALL:CONNected:HSSCchannel2[:SLEVel]:HSPA command.

See Connected DL Channel Levels .

Setting

Range: 1|ON|0|OFF

Query

Range: 1|0

*RST Setting

0 (off)

Requirements

Test Application Revision A.12 and above, with the required feature license.

Lab Application Revision: E.00.16 and above.

Programming Example

 
OUTPUT 714;"CALL:CONNected:HSSCchannel2:STATe:HSPA ON" 

CALL:CONNected:HSSCchannel3[:SLEVel]

Function

The setting form of this command performs two functions: (1) sets the HSDPA Cell 1 Connected HS-SCCH 3 Level (see CALL:CONNected:HSSCchannel3:LEVel ) and (2) sets the HSDPA Cell 1 Connected HS-SCCH 3 Level state to on (see CALL:CONNected:HSSCchannel3:STATe ).

The query form of this command returns the HSDPA Cell 1 Connected HS-SCCH 3 Level .

See Connected DL Channel Levels .

Setting

Range: -20.00 dB to 0 dB

Resolution: 0.01

Query

Same as setting

*RST Setting

-15 dB (off)

Requirements

Test Application Revision: A.08.20 and above, with the required feature license.

Lab Application Revision: C.03 and above

Programming Example

 
OUTPUT 714;"CALL:CONNected:HSSCchannel3 -11"
! Sets the Cell 1 Connected HS-SCCH 3 Level

 to -11 dB and turns its state on.

CALL:CONNected:HSSCchannel3[:SLEVel]:HSPA

Function

The setting form of this command performs two functions: (1) sets the HSPA Cell 1 Connected HS-SCCH 3 Level (see CALL:CONNected:HSSCchannel3:LEVel:HSPA ) and (2) sets the HSPA Cell 1 Connected HS-SCCH 3 Level state to on (see CALL:CONNected:HSSCchannel3:STATe:HSPA ).

The query form of this command returns the HSPA Cell 1 Connected HS-SCCH 3 Level .

See Connected DL Channel Levels .

Setting

Range: -20.00 dB to 0 dB

Resolution: 0.01

Query

Same as setting

*RST Setting

-15 dB (off)

Requirements

Test Application Revision A.12 and above, with the required feature license.

Lab Application Revision: E.00.16 and above.

Programming Example

 
OUTPUT 714;"CALL:CONNected:HSSCchannel3:HSPA -11"
! Sets the HSPA Cell 1 Connected HS-SCCH 3 Level

 to -11 dB and turns its state on.

CALL:CONNected:HSSCchannel3:LEVel

Function

Sets/queries the HSDPA Cell 1 Connected HS-SCCH 3 Level .

The HSDPA Cell 1 Connected HS-SCCH 3 Level can also be set using the CALL:CONNected:HSSCchannel3[:SLEVel] command.

See Connected DL Channel Levels .

Setting

Range: -20.00 dB to 0 dB

Resolution: 0.01

Query

Same as setting

*RST Setting

-15 dB

Requirements

Test Application Revision: A.08.20 and above, with the required feature license.

Lab Application Revision: C.03 and above

Programming Example

 
OUTPUT 714;"CALL:CONNected:HSSCchannel3:LEVel -11"

CALL:CONNected:HSSCchannel3:LEVel:HSPA

Function

Sets/queries the HSPA Cell 1 Connected HS-SCCH 3 Level .

The HSPA Cell 1 Connected HS-SCCH 3 Level can also be set using the CALL:CONNected:HSSCchannel3[:SLEVel]:HSPA command.

See Connected DL Channel Levels .

Setting

Range: -20.00 dB to 0 dB

Resolution: 0.01

Query

Same as setting

*RST Setting

-15 dB

Requirements

Test Application Revision A.12 and above, with the required feature license.

Lab Application Revision: E.00.16 and above.

Programming Example

 
OUTPUT 714;"CALL:CONNected:HSSCchannel3:LEVel:HSPA -11"

CALL:CONNected:HSSCchannel3:STATe

Function

Sets/queries the HSDPA Cell 1 Connected HS-SCCH 3 Level state.

The HSDPA Cell 1 Connected HS-SCCH 3 Level state can also be set using the CALL:CONNected:HSSCchannel3[:SLEVel] command.

See Connected DL Channel Levels .

Setting

Range: 1|ON|0|OFF

Query

Range: 1|0

*RST Setting

0 (off)

Requirements

Test Application Revision: A.08.20 and above, with the required feature license.

Lab Application Revision: C.03 and above

Programming Example

 
OUTPUT 714;"CALL:CONNected:HSSCchannel3:STATe ON" 

CALL:CONNected:HSSCchannel3:STATe:HSPA

Function

Sets/queries the HSPA Cell 1 Connected HS-SCCH 3 Level state.

The HSPA Cell 1 Connected HS-SCCH 3 Level state can also be set using the CALL:CONNected:HSSCchannel3[:SLEVel]:HSPA command.

See Connected DL Channel Levels .

Setting

Range: 1|ON|0|OFF

Query

Range: 1|0

*RST Setting

0 (off)

Requirements

Test Application Revision A.12 and above, with the required feature license.

Lab Application Revision: E.00.16 and above.

Programming Example

 
OUTPUT 714;"CALL:CONNected:HSSCchannel3:STATe:HSPA ON" 

CALL:CONNected:HSSCchannel4[:SLEVel]

Function

The setting form of this command performs two functions: (1) sets the HSDPA Cell 1 Connected HS-SCCH 4 Level (see CALL:CONNected:HSSCchannel4:LEVel ) and (2) sets the HSDPA Cell 1 Connected HS-SCCH 4 Level state to on (see CALL:CONNected:HSSCchannel4:STATe ).

The query form of this command returns the HSDPA Cell 1 Connected HS-SCCH 4 Level .

See Connected DL Channel Levels .

Setting

Range: -20.00 dB to 0 dB

Resolution: 0.01

Query

Same as setting

*RST Setting

-15 dB (off)

Requirements

Test Application Revision: A.08.20 and above, with the required feature license.

Lab Application Revision: C.03 and above

Programming Example

 
OUTPUT 714;"CALL:CONNected:HSSCchannel4 -11"
! Sets the Cell 1 Connected HS-SCCH 4 Level

 to -11 dB and turns its state on.

CALL:CONNected:HSSCchannel4[:SLEVel]:HSPA

Function

The setting form of this command performs two functions: (1) sets the HSPA Cell 1 Connected HS-SCCH 4 Level (see CALL:CONNected:HSSCchannel4:LEVel:HSPA ) and (2) sets the HSPA Cell 1 Connected HS-SCCH 4 Level state to on (see CALL:CONNected:HSSCchannel4:STATe:HSPA ).

The query form of this command returns the HSPA Cell 1 Connected HS-SCCH 4 Level .

See Connected DL Channel Levels .

Setting

Range: -20.00 dB to 0 dB

Resolution: 0.01

Query

Same as setting

*RST Setting

-15 dB (off)

Requirements

Test Application Revision A.12 and above, with the required feature license.

Lab Application Revision: E.00.16 and above.

Programming Example

 
OUTPUT 714;"CALL:CONNected:HSSCchannel4:HSPA -11"
! Sets the HSPA Cell 1 Connected HS-SCCH 4 Level

 to -11 dB and turns its state on.

CALL:CONNected:HSSCchannel4:LEVel

Function

Sets/queries the HSDPA Cell 1 Connected HS-SCCH 4 Level .

The HSDPA Cell 1 Connected HS-SCCH 4 Level can also be set using the CALL:CONNected:HSSCchannel4[:SLEVel] command.

See Connected DL Channel Levels .

Setting

Range: -20.00 dB to 0 dB

Resolution: 0.01

Query

Same as setting

*RST Setting

-15 dB

Requirements

Test Application Revision: A.08.20 and above, with the required feature license.

Lab Application Revision: C.03 and above

Programming Example

 
OUTPUT 714;"CALL:CONNected:HSSCchannel4:LEVel -11"

CALL:CONNected:HSSCchannel4:LEVel:HSPA

Function

Sets/queries the HSPA Cell 1 Connected HS-SCCH 4 Level .

The HSPA Cell 1 Connected HS-SCCH 4 Level can also be set using the CALL:CONNected:HSSCchannel4[:SLEVel]:HSPA command.

See Connected DL Channel Levels .

Setting

Range: -20.00 dB to 0 dB

Resolution: 0.01

Query

Same as setting

*RST Setting

-15 dB

Requirements

Test Application Revision A.12 and above, with the required feature license.

Lab Application Revision: E.00.16 and above.

Programming Example

 
OUTPUT 714;"CALL:CONNected:HSSCchannel4:LEVel:HSPA -11"

CALL:CONNected:HSSCchannel4:STATe

Function

Sets/queries the HSDPA Cell 1 Connected HS-SCCH 4 Level state.

The HSDPA Cell 1 Connected HS-SCCH 4 Level state can also be set using the CALL:CONNected:HSSCchannel4[:SLEVel] command.

See Connected DL Channel Levels .

Setting

Range: 1|ON|0|OFF

Query

Range: 1|0

*RST Setting

0 (off)

Requirements

Test Application Revision: A.08.20 and above, with the required feature license.

Lab Application Revision: C.03 and above

Programming Example

 
OUTPUT 714;"CALL:CONNected:HSSCchannel4:STATe ON" 

CALL:CONNected:HSSCchannel4:STATe:HSPA

Function

Sets/queries the HSPA Cell 1 Connected HS-SCCH 4 Level state.

The HSPA Cell 1 Connected HS-SCCH 4 Level state can also be set using the CALL:CONNected:HSSCchannel4[:SLEVel]:HSPA command.

See Connected DL Channel Levels .

Setting

Range: 1|ON|0|OFF

Query

Range: 1|0

*RST Setting

0 (off)

Requirements

Test Application Revision A.12 and above, with the required feature license.

Lab Application Revision: E.00.16 and above.

Programming Example

 
OUTPUT 714;"CALL:CONNected:HSSCchannel4:STATe:HSPA ON" 

CALL:CONNected:LIMit[:STATe][:SELected]

Function

Sets/queries the call limit state for current selected format (only WCDMA format is available now).

When the call limit state is on, the test set does not respond to PRACH preambles for paging responses from the UE. It forces the UE to repeatedly send PRACH preambles.

Setting

Range: 1|ON|0|OFF

Query

Range: 1|0

*RST Setting

0 (OFF)

Requirements

Test Application Revision: A.03 and above.

Lab Application Revision: A.01 and above

Programming Example

 
OUTPUT 714;"CALL:CONNECTED:LIMIT:STATE 1"

CALL:CONNected:LIMit[:STATe]:WCDMa

Function

Sets/queries the call limit state for the WCDMA format, whether or not that format is active.

When the call limit state is on, the test set does not respond to PRACH preambles from the UE. This allows you to make power measurements on the PRACH preambles.

Setting

Range: 1|ON|0|OFF

Query

Range: 1|0

*RST Setting

0 (OFF)

Requirements

Test Application Revision: A.03 and above.

Lab Application Revision: A.01 and above

Programming Example

 
OUTPUT 714;"CALL:CONNECTED:LIMIT:STATE:WCDMA 1"

CALL:CONNected:PICHannel[:SLEVel]

Function

The setting form of this command performs two functions: (1) sets the Cell 1 Connected PICH Level (see CALL:CONNected:PICHannel:LEVel ) and (2) sets the Cell 1 Connected PICH state to on (see CALL:CONNected:PICHannel:STATe ).

The query form of this command returns the Cell 1 Connected PICH Level .

See Connected DL Channel Levels .

Setting

Range: -20.00 dB to 0 dB

Resolution: 0.01

Query

Same as setting

*RST Setting

-8.33 dB (on)
Requirements

Test Application Revision: A.02 and above.

Lab Application Revision: A.01 and above

Programming Example

 
OUTPUT 714;"CALL:CONNected:PICHannel -7"
! Sets PICH connected power offset to -7 dB and turns its state on.

CALL:CONNected:PICHannel[:SLEVel]:HSDPa

Function

The setting form of this command performs two functions: (1) sets the HSDPA Cell 1 Connected PICH Level (see CALL:CONNected:PICHannel:LEVel:HSDPa ) and (2) sets the HSDPA Cell 1 Connected PICH state to on (see CALL:CONNected:PICHannel:STATe:HSDPa ).

The query form of this command returns the HSDPA Cell 1 Connected PICH Level .

See Connected DL Channel Levels .

Setting

Range: -20.00 dB to 0 dB

Resolution: 0.01

Query

Same as setting

*RST Setting

-15 dB (on)
Requirements

Test Application Revision: A.08.20 and above, with the required feature license.

Lab Application Revision: C.03 and above

Programming Example

 
OUTPUT 714;"CALL:CONNected:PICHannel:HSDPa -7"
! Sets HSDPA PICH connected power offset to -7 dB and turns its state on.

CALL:CONNected:PICHannel[:SLEVel]:HSPA

Function

The setting form of this command performs two functions: (1) sets the HSPA Cell 1 Connected PICH Level (see CALL:CONNected:PICHannel:LEVel:HSPA ) and (2) sets the HSPA Cell 1 Connected PICH state to on (see CALL:CONNected:PICHannel:STATe:HSPA ).

The query form of this command returns the HSPA Cell 1 Connected PICH Level .

See Connected DL Channel Levels .

Setting

Range: -20.00 dB to 0 dB

Resolution: 0.01

Query

Same as setting

*RST Setting

-15 dB (on)
Requirements

Test Application Revision A.12 and above, with the required feature license.

Lab Application Revision: E.00.16 and above.

Programming Example

 
OUTPUT 714;"CALL:CONNected:PICHannel:HSPA -7"
! Sets HSDPA PICH connected power offset to -7 dB and turns its state on.

CALL:CONNected:PICHannel:LEVel

Function

Sets/queries the Cell 1 Connected PICH Level .

The Cell 1 Connected PICH Level can also be set using the CALL:CONNected:PICHannel[:SLEVel] command.

See Connected DL Channel Levels .

Setting

Range: -20.00 dB to 0 dB

Resolution: 0.01

Query

Same as setting

*RST Setting

-8.33 dB
Requirements

Test Application Revision: A.02 and above.

Lab Application Revision: A.01 and above

Programming Example

 
OUTPUT 714;"CALL:CONNected:PICHannel:LEVEL -7"

CALL:CONNected:PICHannel:LEVel:HSDPa

Function

Sets/queries the HSDPA Cell 1 Connected PICH Level .

The HSDPA Cell 1 Connected PICH Level can also be set using the CALL:CONNected:PICHannel[:SLEVel]:HSDPa command.

See Connected DL Channel Levels .

Setting

Range: -20.00 dB to 0 dB

Resolution: 0.01

Query

Same as setting

*RST Setting

-15 dB
Requirements

Test Application Revision: A.08.20 and above, with the required feature license.

Lab Application Revision: C.03 and above

Programming Example

 
OUTPUT 714;"CALL:CONNected:PICHannel:LEVEL:HSDPa -7"

CALL:CONNected:PICHannel:LEVel:HSPA

Function

Sets/queries the HSPA Cell 1 Connected PICH Level .

The HSPA Cell 1 Connected PICH Level can also be set using the CALL:CONNected:PICHannel[:SLEVel]:HSPA command.

See Connected DL Channel Levels .

Setting

Range: -20.00 dB to 0 dB

Resolution: 0.01

Query

Same as setting

*RST Setting

-15 dB
Requirements

Test Application Revision A.12 and above, with the required feature license.

Lab Application Revision: E.00.16 and above.

Programming Example

 
OUTPUT 714;"CALL:CONNected:PICHannel:LEVEL:HSPA -7"

CALL:CONNected:PICHannel:STATe

Function

Sets/queries the Cell 1 Connected PICH state.

The Cell 1 Connected PICH state can also be set using the CALL:CONNected:PICHannel:STATe command.

See Connected DL Channel Levels .

Setting

Range: 1|ON|0|OFF

Query

Range: 1|0

*RST Setting

1 (ON)
Requirements

Test Application Revision: A.02 and above.

Lab Application Revision: A.01 and above

Programming Example

 
OUTPUT 714;"CALL:CONNected:PICHannel:STATe OFF" 

CALL:CONNected:PICHannel:STATe:HSDPa

Function

Sets/queries the HSDPA Cell 1 Connected PICH state.

The HSDPA Cell 1 Connected PICH state can also be set using the CALL:CONNected:PICHannel:STATe:HSDPa command.

See Connected DL Channel Levels .

Setting

Range: 1|ON|0|OFF

Query

Range: 1|0

*RST Setting

1 (ON)
Requirements

Test Application Revision: A.08.20 and above, with the required feature license.

Lab Application Revision: C.03 and above

Programming Example

 
OUTPUT 714;"CALL:CONNected:PICHannel:STATe:HSDPa OFF" 

CALL:CONNected:PICHannel:STATe:HSPA

Function

Sets/queries the HSPA Cell 1 Connected PICH state.

The HSPA Cell 1 Connected PICH state can also be set using the CALL:CONNected:PICHannel:STATe:HSPA command.

See Connected DL Channel Levels .

Setting

Range: 1|ON|0|OFF

Query

Range: 1|0

*RST Setting

1 (ON)
Requirements

Test Application Revision A.12 and above, with the required feature license.

Lab Application Revision: E.00.16 and above.

Programming Example

 
OUTPUT 714;"CALL:CONNected:PICHannel:STATe:HSPA OFF" 

CALL:CONNected:TIMeout

Function

Sets/queries the maximum time the test set will wait for a hanging CALL:CONNected:STATe? query to complete. Default setting units are seconds. To set timeout time in units other than seconds, include an optional unit specifier in the command string.

A timeout timer is started whenever the call-state-change detector becomes armed or gets rearmed when already armed. The duration of this timeout is set using the CALL:CONNected:TIMeout command and should be greater than the maximum amount of time the control program needs to wait between arming the call-state-change detector and the connect/disconnect operation starting. Once the process starts and the call state has moved to one of the transitory states, the W-CDMA defined protocol timers take over and prevent the call state from staying in a transitory state forever. See Call Processing State Synchronization .

Setting

Range: 0 to 100 seconds
Resolution: 0.1 seconds

Query

Range:   0 to 100 seconds
Resolution: 0.1 seconds

*RST Setting

10 seconds

Requirements

Test Application Revision: A.02 and above.

Lab Application Revision: A.01 and above

Programming Example

 
OUTPUT 714;"CALL:CONNECTED:TIMEOUT 3"
! Sets the CALL:CONNected:STATe? query timeout time to 3 seconds.
 
OUTPUT 714;"CALL:CONNECTED:TIMEOUT 500 MS"
! Sets the Sets the CALL:CONNected:STATe? query timeout time to 500 milliseconds.