CALL:HSSCchannel

CALL:HSSCchannel

Last updated: January 14, 2010

This section is only applicable to the lab application or feature-licensed test application.

GPIB Command Conventions

CALL:HSSCchannel[1]:CCODe

Function

THIS COMMAND IS OBSOLETE. Please use CALL:HSSCchannel[1]:CCODe:CODE .

Sets/queries the HS-SCCH 1 Channelization Code .

Setting

Range: CODE2|CODE6|CODE9|CODE10|CODE11|CODE16|CODE17

Query

Same as setting.

*RST Setting

CODE2

Requirements

Test Application Revision: A.08 and above, with the required feature license

Lab Application Revision: C.03 and above.

Programming Example

 
OUTPUT 714;"CALL:HSSCchannel:CCODe CODE11" 
! Sets the HS-SCCH 1 Channelization Code to 11.

CALL:HSSCchannel[1]:CCODe:CODE

Function

Sets/queries the HS-SCCH 1 Channelization Code .

This parameter can not be changed in active cell operating mode (use cell off operating mode or FDD test operating mode to change this parameter).

Setting

Range: 1 to 127

Query

Same as setting.

*RST Setting

2

Requirements

Lab Application Revision: F.00 and above

Test Application Revision: A.14 and above, with the required feature license

Programming Example

 
OUTPUT 714;"CALL:HSSCchannel:CCODe:CODE 2" 
! Sets the HS-SCCH 1 Channelization Code to 2.

CALL:HSSCchannel[1]:CONFig:STATe

Function

Sets/queries the FDD Test Mode HSDPA/HSPA HS-SCCH 1 Channel Configuration State.

Setting

Range: 1|ON|0|OFF

Query

Range: 0|1

*RST Setting

1 (ON)
Requirements

Lab Application Revision: F.00 and above

Test Application Revision: A.14 and above, with the required feature license

Programming Example

 
OUTPUT 714;"CALL:HSSCchannel:CONFig:STATe" 
!Sets the FDD Test Mode HSDPA/HSPA HS-SCCH 1 Channel Configuration State.to on.

CALL:HSSCchannel2:CCODe

Function

THIS COMMAND IS OBSOLETE. Please use CALL:HSSCchannel2:CCODe:CODE .

Sets/queries the HS-SCCH 2 Channelization Code .

Setting

Range: CODE2|CODE6|CODE9|CODE10|CODE11|CODE16|CODE17

Query

Same as setting.

*RST Setting

CODE6

Requirements

Test Application Revision: A.08 and above, with the required feature license

Lab Application Revision: C.03 and above.

Programming Example

 
OUTPUT 714;"CALL:HSSCchannel2:CCODe CODE11" 
! Sets the HS-SCCH 2 Channelization Code to 11.

CALL:HSSCchannel2:CCODe:CODE

Function

Sets/queries the HS-SCCH 2 Channelization Code .

This parameter can not be changed in active cell operating mode (use cell off operating mode or FDD test operating mode to change this parameter).

Setting

Range: 1 to 127

Query

Same as setting.

*RST Setting

6

Requirements

Lab Application Revision: F.00 and above

Test Application Revision: A.14 and above, with the required feature license

Programming Example

 
OUTPUT 714;"CALL:HSSCchannel2:CCODe:CODE 6" 
! Sets the HS-SCCH 2 Channelization Code to 6.

CALL:HSSCchannel2:CONFig:STATe

Function

Sets/queries the FDD Test Mode HSDPA/HSPA HS-SCCH 2 Channel Configuration State.

Setting

Range: 1|ON|0|OFF

Query

Range: 0|1

*RST Setting

1 (ON)
Requirements

Lab Application Revision: F.00 and above

Test Application Revision: A.14 and above, with the required feature license

Programming Example

 
OUTPUT 714;"CALL:HSSCchannel2:CONFig:STATe" 
!Sets the FDD Test Mode HSDPA/HSPA HS-SCCH 2 Channel Configuration State.to on.

CALL:HSSCchannel3:CCODe

Function

THIS COMMAND IS OBSOLETE. Please use CALL:HSSCchannel3:CCODe:CODE .

Sets/queries the HS-SCCH 3 Channelization Code .

Setting

Range: CODE2|CODE6|CODE9|CODE10|CODE11|CODE16|CODE17

Query

Same as setting.

*RST Setting

CODE9

Requirements

Test Application Revision: A.08 and above, with the required feature license

Lab Application Revision: C.03 and above.

Programming Example

 
OUTPUT 714;"CALL:HSSCchannel3:CCODe CODE11" 
! Sets the HS-SCCH 3 Channelization Code to 11.

CALL:HSSCchannel3:CCODe:CODE

Function

Sets/queries the HS-SCCH 3 Channelization Code .

This parameter can not be changed in active cell operating mode (use cell off operating mode or FDD test operating mode to change this parameter).

Setting

Range: 1 to 127

Query

Same as setting.

*RST Setting

9

Requirements

Lab Application Revision: F.00 and above

Test Application Revision: A.14 and above, with the required feature license

Programming Example

 
OUTPUT 714;"CALL:HSSCchannel3:CCODe:CODE 9" 
! Sets the HS-SCCH 3 Channelization Code to 9.

CALL:HSSCchannel3:CONFig:STATe

Function

Sets/queries the FDD Test Mode HSDPA/HSPA HS-SCCH 3 Channel Configuration State.

Setting

Range: 1|ON|0|OFF

Query

Range: 0|1

*RST Setting

1 (ON)
Requirements

Lab Application Revision: F.00 and above

Test Application Revision: A.14 and above, with the required feature license

Programming Example

 
OUTPUT 714;"CALL:HSSCchannel3:CONFig:STATe" 
!Sets the FDD Test Mode HSDPA/HSPA HS-SCCH 3 Channel Configuration State.to on.

CALL:HSSCchannel4:CCODe

Function

THIS COMMAND IS OBSOLETE. Please use CALL:HSSCchannel4:CCODe:CODE .

Sets/queries the HS-SCCH 4 Channelization Code .

Setting

Range: CODE2|CODE6|CODE9|CODE10|CODE11|CODE16|CODE17

Query

Same as setting.

*RST Setting

CODE10

Requirements

Test Application Revision: A.08 and above, with the required feature license

Lab Application Revision: C.03 and above.

Programming Example

 
OUTPUT 714;"CALL:HSSCchannel4:CCODe CODE11" 
! Sets the HS-SCCH 4 Channelization Code to 11.

CALL:HSSCchannel4:CCODe:CODE

Function

Sets/queries the HS-SCCH 4 Channelization Code .

This parameter can not be changed in active cell operating mode (use cell off operating mode or FDD test operating mode to change this parameter).

Setting

Range: 1 to 127

Query

Same as setting.

*RST Setting

10

Requirements

Lab Application Revision: F.00 and above

Test Application Revision: A.14 and above, with the required feature license

Programming Example

 
OUTPUT 714;"CALL:HSSCchannel4:CCODe:CODE 10" 
! Sets the HS-SCCH 4 Channelization Code to 10.

CALL:HSSCchannel4:CONFig:STATe

Function

Sets/queries the FDD Test Mode HSDPA/HSPA HS-SCCH 4 Channel Configuration State.

Setting

Range: 1|ON|0|OFF

Query

Range: 0|1

*RST Setting

1 (ON)
Requirements

Lab Application Revision: F.00 and above

Test Application Revision: A.14 and above, with the required feature license

Programming Example

 
OUTPUT 714;"CALL:HSSCchannel4:CONFig:STATe" 
!Sets the FDD Test Mode HSDPA/HSPA HS-SCCH 4 Channel Configuration State.to on.