CALL:SCODe

CALL:SCODe

Last updated: January 16, 2009

GPIB Command Conventions

CALL[:CELL]:SCODe[:PRIMary]

Function

Sets/queries the primary scrambling code.

The actual code number for the primary scrambling code is 16 times the value of this setting. See 3GPP TS 25.213, "Spreading and Modulation (FDD)" for a complete description of the relationship between this index and the actual spreading code number.

This setting cannot be changed while the active cell operating mode. Attempting to change this setting while in this mode will result in the following error message: "Command Rejected. Change Not Allowed in Active Cell Mode." Use the cell off operating mode when changing this setting.

Setting

Range: 0 to 511

Query

Range: 0 to 511

*RST Setting

0

Requirements

Test or Lab Application Revision: A.01 and above

Programming Example

 
OUTPUT 714;"CALL:CELL:SCODe 10" !Sets the primary scrambling code to 10.