What 3GPP W-CDMA/HSPA Conformance Tests Are Supported?

Last updated: October 30, 2013

These tables list the tests specified in 3GPP TS 34.121, whether the tests are supported by the test set, and the recommended measurement to perform the tests.

3GPP TS 34.121 Section 5 Transmitter Characteristics

3GPP TS 34.121

Test Description

Supported in Test Set? Measurement Procedure

5.2

Maximum Output Power

Yes

How Do I Make a Thermal Power Measurement?
5.2A Maximum Output Power with HS-DPCCH (Release 5 only)

Yes#

How Do I Make a Channel Power Measurement?
5.2AA Maximum Output Power with HS-DPCCH (Release 6 and later)

Yes#

How Do I Make a Channel Power Measurement?
5.2B Maximum Output Power with HS-DPCCH and E-DCH

Yes#

How Do I Make a Channel Power Measurement?
5.2C UE Relative Code Domain Power Accuracy

Yes#

Measuring 3GPP TS 34.121-1 (v8.10.0) 5.2C UE Relative Code Domain Power Accuracy for HS-DPCCH
5.2D UE Relative Code Domain Power Accuracy for HS-DPCCH and E-DCH

Yes#

Measuring 3GPP TS 34.121-1 (v8.10.0) 5.2D UE Relative Code Domain Power Accuracy for HS-DPCCH and E-DCH
5.2E

UE Relative Code Domain Power Accuracy for HS-DPCCH and E-DCH with 16QAM

Yes#

Measuring 3GPP TS 34.121-1 (v8.10.0) s5.2E UE Relative Code Domain Power Accuracy for HS-DPCCH and E-DCH with 16QAM

5.3

Frequency Error

Yes

How Do I Make a Waveform Quality Measurement?

5.4.1

Open Loop Power Control in the Uplink

Yes

How Do I Make a PRACH Transmit On/Off Power Measurement?

5.4.2

Inner Loop Power Control in the Uplink

Partially

How Do I Make an Inner Loop Power Measurement? (does not support 3 dB step size)

5.4.3

Minimum Output Power

Yes

How Do I Make a Channel Power Measurement? (with RRC filter OFF)

5.4.4

Out-of-synchronization handling of output power

Yes +, ** How Do I Make an Out-of-Synch Handling of Output Power Measurement? (Establish a connection between the test set and UE, initiate the measurement from the test set, measure the UE's output power using the spectrum analyzer)

5.5.1

Transmit OFF Power

Yes

How Do I Make a PRACH Transmit On/Off Power Measurement?

5.5.2

Transmit ON/OFF Time mask

Yes

How Do I Make a PRACH Transmit On/Off Power Measurement?

5.6

Change of TFC

Yes + How Do I Make a Change of TFC (Transport Format Combination) Measurement?

5.7

Power setting in uplink compressed mode

No  
5.7A HS-DPCCH

Yes#

How Do I Make a Dynamic Power Analysis Measurement?

5.8

Occupied Bandwidth (OBW)

Yes

How Do I Make an Occupied Bandwidth (OBW) Measurement?

5.9

Spectrum Emission Mask

Yes

How Do I Make a Spectrum Emission Mask Measurement?
5.9A Spectrum Emission Mask with HS-DPCCH

Yes#

How Do I Make a Spectrum Emission Mask Measurement?
5.9B Spectrum Emission Mask with E-DCH

Yes#

How Do I Make a Spectrum Emission Mask Measurement?

5.10

Adjacent Channel Leakage Power Ratio (ACLR)

Yes

How Do I Make an Adjacent Channel Leakage Ratio (ACLR) Measurement?
5.10A

Adjacent Channel Leakage Power Ratio (ACLR) with HS-DPCCH

Yes#

How Do I Make an Adjacent Channel Leakage Ratio (ACLR) Measurement?
5.10B

Adjacent Channel Leakage Power Ratio (ACLR) with E-DCH

Yes#

How Do I Make an Adjacent Channel Leakage Ratio (ACLR) Measurement?

5.11

Spurious Emissions

Yes**

Camp to test set, measure spurious emissions using external spectrum analyzer

5.12

Transmit Intermodulation

Yes* , ** Camp to the test set, inject tones using external signal generator, measure transmit intermodulation using external spectrum analyzer

5.13.1

Error Vector Magnitude (EVM)

Yes

How Do I Make a Waveform Quality Measurement?

5.13.1A

Error Vector Magnitude (EVM) with HS-DPCCH

Yes#

How Do I Make a Waveform Quality Measurement?
5.13.1AA

Error Vector Magnitude (EVM) and Phase Discontinuity with HS-DPCCH

Yes#

How Do I Make a Phase Discontinuity Measurement?
5.13.1AAA

EVM and IQ origin offset for HS-DPCCH and E-DCH with 16 QAM

Yes # Measuring 3GPP TS 34.121-1 (v8.10.0) s5.13.1AAA EVM and IQ origin offset for HS-DPCCH and E-DCH with 16 QAM

5.13.2

Peak code domain error

Partially How Do I Make a Waveform Quality Measurement? (only for a single DPCH)
5.13.2A Relative Code Domain Error with HS-DPCCH

Yes#

Measuring 3GPP TS 34.121-1 (v8.10.0) s5.13.2A Relative Code Domain Error for HS-DPCCH
5.13.2B Relative Code Domain Error with HS-DPCCH and E-DCH

Yes#

Measuring 3GPP TS 34.121-1 (v8.10.0) s5.13.2B Relative Code Domain Error for HS-DPCCH and E-DCH
5.13.2C

Relative Code Domain Error for HS-DPCCH and E-DCH with 16QAM

Yes#

Measuring 3GPP TS 34.121-1 (v8.10.0) s5.13.2C Relative Code Domain Error for HS-DPCCH and E-DCH with 16QAM
5.13.3 UE Phase Discontinuity Yes How Do I Make a Phase Discontinuity Measurement?
5.13.4 PRACH Preamble Quality Partially +

How Do I Make a PRACH Preamble Analysis Measurement? (measurement is not performed on first preamble, AICH transmission timing is fixed to 0, measurement does not determine if correct access slot was used)

3GPP TS 34.121 Section 6 Receiver Characteristics

3GPP TS 34.121

Test Description

Supported in Test Set? Measurement Procedure

6.2

Reference Sensitivity Level

Yes

How Do I Make a Loopback Bit Error Ratio (BER) Measurement?

6.2A

Reference Sensitivity Level for DC-HSDPA

Yes#

6.2B

Reference Sensitivity Level for DB-DC-HSDPA

Yes#

6.3

Maximum Input Level

Yes

How Do I Make a Loopback Bit Error Ratio (BER) Measurement?
6.3A

Maximum Input Level for HS-PDSCH Reception (16QAM)

Yes#

Measuring 3GPP TS 34.121-1 6.3A Maximum Input Level for HS-PDSCH Reception (16QAM)

6.3B

Maximum Input Level for HS-PDSCH Reception (64QAM)

Yes#

Measuring 3GPP TS 34.121-1 6.3B Maximum Input Level for HS-PDSCH Reception (64QAM)

6.3C

Maximum Input Level for DC-HSDPA Reception (16QAM)

Yes#

Measuring 3GPP TS 34.121-1 6.3C Maximum Input Level for DC-HSDPA Reception (16QAM)

6.3D

Maximum Input Level for DC-HSDPA Reception (64QAM)

Yes#

Measuring 3GPP TS 34.121-1 6.3D Maximum Input Level for DC-HSDPA Reception (64QAM)

6.3E

Maximum Input Level for DB-DC-HSDPA Reception (16QAM)

Yes#

6.3F

Maximum Input Level for DB-DC-HSDPA Reception (64QAM)

Yes#

6.4

Adjacent Channel Selectivity (ACS) (Rel-99 and Rel-4)

Yes*

How Do I Make a Loopback Bit Error Ratio (BER) Measurement? (plus W-CDMA signal from a signal generator)

6.4A

Adjacent Channel Selectivity (ACS) (Rel-5 and later releases)

Yes*

How Do I Make a Loopback Bit Error Ratio (BER) Measurement? (plus W-CDMA signal from a signal generator)

6.4B

Adjacent channel selectivity (ACS) for DC-HSDPA

Yes*

6.4C

Adjacent channel selectivity (ACS) for DB-DC-HSDPA

Yes*

6.5

Blocking Characteristics

Yes*

How Do I Make a Loopback Bit Error Ratio (BER) Measurement? (plus W-CDMA signal from a signal generator)

6.5A

Blocking characteristics for DC-HSDPA

Yes*

6.5B

Blocking characteristics for DB-DC-HSDPA

Yes*

6.6

Spurious Response

Yes*

How Do I Make a Loopback Bit Error Ratio (BER) Measurement? (plus a CW signal from a signal generator)

6.6A

Spurious response for DC-HSDPA

Yes*

6.6B

Spurious response for DB-DC-HSDPA

Yes*

6.7

Intermodulation Characteristics

Yes*

How Do I Make a Loopback Bit Error Ratio (BER) Measurement? (plus 2 CW signals from signal generators)

6.7A

Intermodulation characteristics for DC-HSDPA

Yes*

6.7B

Intermodulation characteristics for DB-DC-HSDPA

Yes*

6.8

Spurious Emissions

Yes**

Camp to test set, measure spurious emissions using external spectrum analyzer
3GPP TS 34.121 Section 7 Performance Requirements
3GPP TS 34.121 Test Description Supported in Test Set? Measurement Procedure
7.2.1 Demodulation in Static Propagation Conditions: Demodulation of Dedicated Channel (DCH) Yes How Do I Make a Block Error Ratio (BLER) Measurement?
7.3.1 Demodulation of DCH in Multi-Path Fading Propagation Conditions: Single Link Performance Partially +, *** How Do I Make a Block Error Ratio (BLER) Measurement? (plus multi-path fading simulator and external AWGN noise source) (only for tests with phase reference = P-CPICH)
7.4.1 Demodulation of DCH in Moving Propagation Conditions: Single Link Performance Yes +, *** How Do I Make a Block Error Ratio (BLER) Measurement? (plus multi-path fading simulator and external AWGN noise source)
7.5.1 Demodulation of DCH in Birth-Death Propagation Conditions: Single Link Performance Yes +, *** How Do I Make a Block Error Ratio (BLER) Measurement? (plus multi-path fading simulator and external AWGN noise source)

7.5.1A

Demodulation of DCH in high speed train condition

Yes +, *** How Do I Make a Block Error Ratio (BLER) Measurement? (plus multi-path fading simulator and external AWGN noise source)
7.6.1 Demodulation of DCH in Open-Loop Transmit Diversity Mode No  
7.6.2 Demodulation of DCH in Closed Loop Transmit Diversity Mode No  
7.6.3 Demodulation of DCH in Site Selection Diversity Transmission Power Control Mode No  
7.7.1 Demodulation of DCH in Inter-Cell Soft Handover Yes +, ***  

7.7.1A

Demodulation of DCH in Inter-Cell Soft Handover (Release 6 and later)

Yes +, ***

7.7.2 Combining of TPC Commands from Radio Links of Different Radio Link Sets No  
7.7.3 Combining of Reliable TPC Commands from Radio Links of Different Radio Link Sets No

7.8.1 Power Control in the Downlink, Constant BLER Target No  

7.8.1A

Power control in the downlink, constant BLER target (Release 6 and later)

Yes

7.8.2 Power Control in the Downlink, Initial Convergence No  
7.8.3 Power Control in the Downlink, Wind Up Effects No  

7.8.3A

Power control in the downlink, wind up effects (Release 6 and later)

Yes

7.8.4 Power Control in the Downlink, Different Transport Formats Yes

7.8.5

Power control in the downlink for F-DPCH

No

7.9.1 Downlink Compressed Mode: Single Link Performance No  

7.9.1A

Single link performance (Release 6 and later)

No

7.10 Blind Transport Format Detection No  
7.11 Demodulation of Paging Channel (PCH) No  
7.12 Detection of Acquisition Indicator (AI) No  

7.13

UE UL power control operation with discontinuous UL DPCCH transmission operation

No

3GPP TS 34.121 Section 9 Performance Requirements for HSDPA
3GPP TS 34.121 Test Description Supported in the Test Set? Measurement Procedure
9.2.1A Demodulation of HS-DSCH (Fixed Reference Channel): Single Link Performance - QPSK/16QAM, FRC H-Set 1/2/3 Yes +, *** How Do I Make an HSDPA Block Error Ratio Measurement? (plus multi-path fading simulator and external AWGN noise source)
9.2.1B Demodulation of HS-DSCH (Fixed Reference Channel): Single Link Performance - QPSK, FRC H-Set 4/5 Yes +, *** How Do I Make an HSDPA Block Error Ratio Measurement? (plus multi-path fading simulator and external AWGN noise source)
9.2.1C Demodulation of HS-DSCH (Fixed Reference Channel): Single Link Performance - QPSK/16QAM, FRC H-Set 6/3 Yes +, *** How Do I Make an HSDPA Block Error Ratio Measurement? (plus multi-path fading simulator and external AWGN noise source)
9.2.1D Demodulation of HS-DSCH (Fixed Reference Channel): Single Link Performance - Enhanced Performance Requirements Type 1 - QPSK/16QAM, FRC H-Set 1/2/3 Yes +, *** How Do I Make an HSDPA Block Error Ratio Measurement? (plus multi-path fading simulator and external AWGN noise source)
9.2.1E Demodulation of HS-DSCH (Fixed Reference Channel): Single Link Performance - Enhanced Performance Requirements Type 1 - QPSK/16QAM, FRC H-Set 6/3 Yes +, *** How Do I Make an HSDPA Block Error Ratio Measurement? (plus multi-path fading simulator and external AWGN noise source)
9.2.1F Demodulation of HS-DSCH (Fixed Reference Channel): Single Link Performance - Enhanced Performance Requirements Type 2 - QPSK/16QAM, FRC H-Set 6/3 Yes +, *** How Do I Make an HSDPA Block Error Ratio Measurement? (plus multi-path fading simulator and external AWGN noise source)

9.2.1FA

Single Link Performance - Enhanced Performance Requirements Type 2 - QPSK/16QAM, Fixed Reference Channel (FRC) H-Set 6A/3A

Yes+, ***

9.2.1FB

Single Link Performance - Enhanced Performance Requirements Type 2 - QPSK/16QAM, Fixed Reference Channel (FRC) H-Set 6A/3A for DB-DC-HSDPA

Yes+, ***

9.2.1G Single Link Performance - Enhanced Performance Requirements Type 3 - QPSK/16QAM, Fixed Reference Channel (FRC) H-Set 6/3 Yes +, *** How Do I Make an HSDPA Block Error Ratio Measurement? (plus multi-path fading simulator and external AWGN noise source)

9.2.1GA

Single Link Performance - Enhanced Performance Requirements Type 3 - QPSK/16QAM, Fixed Reference Channel (FRC) H-Set 6A/3A

Yes+, ***

9.2.1GB

Single Link Performance - Enhanced Performance Requirements Type 3 - QPSK/16QAM, Fixed Reference Channel (FRC) H-Set 6A/3A for DB-DC-HSDPA

Yes+, ***

9.2.1H Single Link Performance - Enhanced Performance Requirements Type 2 - 64QAM, Fixed Reference Channel (FRC) H-Set 8 Yes +, *** How Do I Make an HSDPA Block Error Ratio Measurement? (plus multi-path fading simulator and external AWGN noise source)

9.2.1HA

Single Link Performance - Enhanced Performance Requirements Type 2 - 64QAM, Fixed Reference Channel (FRC) H-Set 8A

Yes+, ***

9.2.1HB

Single Link Performance - Enhanced Performance Requirements Type 2 - 64QAM, Fixed Reference Channel (FRC) H-Set 8A for DB-DC-HSDPA

Yes+, ***

9.2.1I Single Link Performance - Enhanced Performance Requirements Type 3 - 64QAM, Fixed Reference Channel (FRC) H-Set 8 Yes +, *** How Do I Make an HSDPA Block Error Ratio Measurement? (plus multi-path fading simulator and external AWGN noise source)

9.2.1IA

Single Link Performance - Enhanced Performance Requirements Type 3 - 64QAM, Fixed Reference Channel (FRC) H-Set 8A

Yes+, ***

9.2.1IB

Single Link Performance - Enhanced Performance Requirements Type 3 - 64QAM, Fixed Reference Channel (FRC) H-Set 8A for DB-DC-HSDPA

Yes+, ***

9.2.1J

Single Link Performance - Enhanced Performance Requirements Type 2 - QPSK/16QAM, Fixed Reference Channel (FRC) H-Set 10

Yes +, *** How Do I Make an HSDPA Block Error Ratio Measurement? (plus multi-path fading simulator and external AWGN noise source)

9.2.1JA

Single Link Performance - Enhanced Performance Requirements Type 2 - QPSK/16QAM, Fixed Reference Channel (FRC) H-Set 10A

Yes+, ***

9.2.1JB

Single Link Performance - Enhanced Performance Requirements Type 2 - QPSK/16QAM, Fixed Reference Channel (FRC) H-Set 10A for DB-DC-HSDPA

Yes+, ***

9.2.1K

Single Link Performance - Enhanced Performance Requirements Type 3 - QPSK/16QAM, Fixed Reference Channel (FRC) H-Set 10

Yes +, *** How Do I Make an HSDPA Block Error Ratio Measurement? (plus multi-path fading simulator and external AWGN noise source)

9.2.1KA

Single Link Performance - Enhanced Performance Requirements Type 3 - QPSK/16QAM, Fixed Reference Channel (FRC) H-Set 10A

Yes+, ***

9.2.1KB

Single Link Performance - Enhanced Performance Requirements Type 3 - QPSK/16QAM, Fixed Reference Channel (FRC) H-Set 10A for DB-DC-HSDPA No

9.2.1LA

Single Link Performance - Enhanced Performance Requirements Type 3i - QPSK, Fixed Reference Channel (FRC) H-Set 6A

Yes+, ***

9.2.1LB

Single Link Performance - Enhanced Performance Requirements Type 3i - QPSK, Fixed Reference Channel (FRC) H-Set 6A for DB-DC-HSDPA

No

9.2.2 Open Loop Diversity Performance No

9.2.3 Closed Loop Diversity Performance No

9.2.4A MIMO Performance - Fixed Reference Channel (FRC) H-Set 9

Yes*, ***

9.2.4B MIMO Performance - Fixed Reference Channel (FRC) H-Set 11

Yes*, ***

9.3.1 Reporting of CQI: Single Link Performance - AWGN Propagation Conditions Yes+ HSDPA Reporting of Channel Quality Indicator Measurement Description

9.3.1A

Reporting of CQI: Single Link Performance - AWGN Propagation Conditions, 64QAM

Yes+ HSDPA Reporting of Channel Quality Indicator Measurement Description

9.3.1B

Single Link Performance - AWGN Propagation Conditions, DC-HSDPA requirements

No

9.3.1BA

Single Link Performance - AWGN Propagation Conditions, DB-DC-HSDPA requirements

No

9.3.2 Reporting of CQI: Single Link Performance - Fading Propagation Conditions No  

9.3.2A

Single Link Performance - Fading Propagation Conditions, DC-HSDPA requirements

No

9.3.2AA

Single Link Performance - Fading Propagation Conditions, DB-DC-HSDPA requirements

No

9.3.3 Reporting of CQI: Open Loop Diversity Performance - AWGN Propagation Conditions No

9.3.4 Reporting of CQI: Open Loop Diversity Performance - Fading Propagation Conditions No

9.3.5 Reporting of CQI: Closed Loop Diversity Performance - AWGN Propagation Conditions No

9.3.6 Reporting of CQI: Closed Loop Diversity Performance - Fading Propagation Conditions No

9.3.7

MIMO Performance - Reporting of Channel Quality Indicator

No

9.4.1 HS-SCCH Detection Performance: Single Link Performance Yes +, *** How Do I Make an HSDPA Block Error Ratio Measurement? (plus multi-path fading simulator and external AWGN noise source) (HS-SCCH 2-4 all use the same Alternate H-RNTI )
9.4.1A HS-SCCH Detection Performance: Single Link Performance - Enhanced Performance Requirements Type 1 Partially +, *** How Do I Make an HSDPA Block Error Ratio Measurement? (plus multi-path fading simulator and external AWGN noise source) (HS-SCCH 2-4 all use the same Alternate H-RNTI )
9.4.2

HS-SCCH Detection Performance: Open Loop Diversity Performance

No

9.4.2A

HS-SCCH Detection Performance: Open Loop Diversity Performance - Enhanced Performance Requirements Type 1

No

9.4.3

HS SCCH Detection Performance: HS-SCCH Type 3 Performance

No

9.5

HS-SCCH-less demodulation of HS-DSCH (Fixed Reference Channel)

No

3GPP TS 34.121 Section 10 Performance Requirement (E-DCH)
3GPP TS 34.121 Test Description Supported in the Test Set? Measurement Procedure
10.2.1.1 Detection of E-DCH HARQ ACK Indicator Channel (E-HICH): Single Link Performance (10 ms TTI) Yes+

10.2.1.2

Detection of E-DCH HARQ ACK Indicator Channel (E-HICH): Single Link Performance (2 ms TTI) Yes+

10.3.1.1 Detection of E-DCH Relative Grant Channel (E-RGCH): Single Link Performance (10 ms TTI) Yes+

10.3.1.2 Detection of E-DCH Relative Grant Channel (E-RGCH): Single Link Performance (2 ms TTI) Yes+

10.4.1 Demodulation of E-DCH Absolute Grant Channel (E-AGCH): Single Link Performance Yes+  

+ This test is supported in the lab application only.

# This test is supported in the lab application or feature-licensed test application only.

* Requires also an external signal generator, such as the E4438C ESG Vector Signal Generator.

** Requires also an external spectrum analyzer, such as the E4445A PSA Spectrum Analyzer.

*** Requires also a multi-path fading simulator and external AWGN source, such as the N5115B Fading Solution.

Related Topics


3GPP Compliance