How Do I Configure and Enable (Start) Event Reporting?

How Do I Configure and Enable (Start) Event Reporting?

Last updated: January 16, 2009

This section is only applicable to the lab application.

A. Configure Event Parameters

  1. Go to the Soft Handover Information Screen

  2. Select SHO / Event Parameters ( F2 ).

  3. Set event parameters as needed.

B. Enable Event Reporting

  1. Go to the Soft Handover Information Screen
  2. Set Event State ( F4 ) to On . The test set sends a Measurement Control message to the UE with the event parameter configuration specified in step A. Configure Event Parameters .

The UE reports events for cell 1 and cell 2 as they occur, as well as MS reported measurement results for each cell.

C. Change Event Parameters

  1. A. Configure Event Parameters .
  2. Select Send Event Config ( F5 if Event State is On ), to send a new Measurement Control message to the UE, specifying the changes to the event parameters.

   
NOTE
You can also send a new Measurement Control message to the UE by toggling Event State off and on.

   

Related Topics


Soft Handover

How Do I Configure Cell 2?

How Do I Perform a Soft Handover?