The MEASure queries are the easiest way to program measurements because they always use default measurement parameters. You set the function, range, and resolution in one command, but you cannot change other parameters from their default values. The results are sent directly to the instrument's output buffer.
A MEASure query is functionally equivalent to sending CONFigure followed immediately by READ?. The difference is that CONFigure commands allow you to change parameters between the CONFigure and the READ? |
MEASure:{RESistance|FRESistance}?
With the MEASure? queries, you can select the function, range and resolution in one command. All other parameters are set to their default values (below).
Measurement Parameter | Default Setting |
---|---|
AC Input Filter (bandwidth) |
20 Hz (medium filter) |
Autozero |
OFF if resolution setting results in NPLC < 1 |
Range |
AUTO (including voltage range for frequency and period measurements) |
Samples per Trigger |
1 sample |
Trigger Count |
1 trigger |
Trigger Delay |
Automatic delay |
Trigger Source |
Immediate |
Trigger Slope |
NEGative |
Math Functions |
Disabled. Other parameters are unchanged. |
Per-function Null State |
Disabled |
The following example configures DC voltage measurements, internally triggers the instrument to take a measurement, and reads the measurement. The default range (autorange) and resolution (10 PLC) are used for the measurement.
MEAS:VOLT:DC?
Typical Response: +4.23450000E-03
The following example configures the instrument for 2-wire resistance measurements, triggers the instrument to take a measurement, and reads the measurement. The 1 kΩ range is selected with 0.1 Ω resolution.
MEAS:RES? 1000,0.1
Typical Response: +3.27150000E+02
Sets all measurement parameters and trigger parameters to their default values for capacitance measurements and immediately triggers a measurement. The results are sent directly to the instrument's output buffer.
Parameter | Typical Return |
---|---|
<range>: {1 nF|10 nF|100 nF|1 µF|10 µF|100 µF}. Default: AUTO. |
(none) |
<resolution>: optional and ignored; fixed at 4½ digits. |
|
Configure capacitance measurements. Then make and read one measurement: MEAS:CAP? Typical Response:+3.01534021E-10 |
Sets all measurement parameters and trigger parameters to their default values for continuity test and immediately triggers a measurement. The results are sent directly to the instrument's output buffer.
Parameter | Typical Return |
---|---|
(none) | (none) |
Configure the instrument for continuity measurements. Then make and read one measurement:
Typical Response: +1.32130000E-02 |
Sets all measurement parameters and trigger parameters to their default values for AC or DC current measurements and immediately triggers a measurement. The results are sent directly to the instrument's output buffer.
Parameter | Typical Return |
---|---|
<range>: {100 µA|1 mA|10 mA|100 mA|1 A|3 A|10 A}. Default: AUTO (autorange). |
(none) |
<resolution> (AC): optional and ignored; fixed at 6½ digits. Specify <resolution> in the measurement's units (V, A, Hz, Ω, and so on). |
|
Configure AC current measurements using the 1 A range. Then make and read one measurement: Typical Response: +8.54430000E-01 |
Sets all measurement parameters and trigger parameters to their default values for diode test measurements and immediately triggers a measurement. The results are sent directly to the instrument's output buffer.
Parameter | Typical Return |
---|---|
(none) | (none) |
Configure, make, and read a default diode measurement: Typical Response:+1.32130000E-01 |
Sets all measurement parameters and trigger parameters to their default values for frequency or period measurements and immediately triggers a measurement. The results are sent directly to the instrument's output buffer.
Parameter | Typical Return |
---|---|
<range>: 3 Hz to 300 kHz. Default: 20 Hz. for FREQuency <range>: 3.33 µs to 333.33 ms. Default: 50 ms (PERiod). |
(none) |
<resolution>: See table below. Specify <resolution> in the measurement's units (V, A, Hz, Ω, and so on). |
|
Configure frequency measurements using the default aperture. Then make and read one measurement: Typical Response:+1.32130000E+03 |
Resolution (34460A/61A) | Resolution (34465A/70A) | Aperture |
---|---|---|
Not Applicable | 100 ppm × <range> (MAXimum) | 1 ms |
100 ppm × <range> (MAXimum) | 10 ppm × <range> (DEFault) | 10 ms |
10 ppm × <range> (DEFault) | 1 ppm × <range> | 100 ms |
1 ppm × <range> (MINimum) | 0.1 ppm × <range> (MINimum) | 1 s |
Sets all measurement and trigger parameters to their default values for 4-wire resistance (FRESistance) or 2-wire (RESistance) measurements, and immediately triggers a measurement. The results are sent directly to the instrument's output buffer.
Parameter | Typical Return |
---|---|
<range>: 100 Ω, 1 kΩ, 10 kΩ, 100 kΩ, 1 MΩ, 10 MΩ, 100 MΩ, 1 GΩ, AUTO,or DEFault. Default: AUTO. | (none) |
<resolution>: See Resolution Table or Range, Resolution and NPLC. The default is equivalent to 10 PLC. Specify <resolution> in the measurement's units (V, A, Hz, Ω, and so on). |
|
Configure 4-wire resistance measurements using the 100 Ω range with default resolution. Then make and read one measurement: Typical Response:+8.54530000E+01 |
Sets all measurement parameters and trigger parameters to their default values for temperature measurements and immediately triggers a measurement. The results are sent directly to the instrument's output buffer.
Parameter | Typical Return |
---|---|
<probe_type>: {FRTD|RTD|FTHermistor|THERmistor|TCouple}. Default: FRTD. |
(none) |
<type>: 85 (only possible value for RTD/FRTD), 5000 (only possible value for THERmistor/FTHermistor), or E, J, K, N, R, T (TCouple). |
|
<resolution>: See Resolution Table or Range, Resolution and NPLC. The default is equivalent to 10 PLC. |
|
Configure a 4-wire RTD measurement with default resolution. Then make and read one measurement: Typical Response:+2.12320000E+01 |
Sets all measurement parameters and trigger parameters to their default values for AC or DC voltage measurements and immediately triggers a measurement. The results are sent directly to the instrument's output buffer.
|
The maximum range parameter (MAX) is 1000 V. However, the SAFETY LIMIT on the front and rear HI/LO input terminals is 750 VAC (rms). The rms voltage is waveform dependent. A sine wave is limited to 750 VAC (rms), but a 1000 Vpk square wave is safe. Connection to AC mains power is further limited to CAT II (300 V). See Safety and Regulatory Information for more information on the safety features and the safe operation of this instrument. |
Parameter | Typical Return |
---|---|
<range>: 100 mV, 1 V, 10 V, 100 V, 1000 V, AUTO (default) or DEFault |
(none) |
<resolution> (AC): optional and ignored; fixed at 6½ digits. <resolution> (DC): See Resolution Table or Range, Resolution and NPLC. The default is equivalent to 10 PLC. Specify <resolution> in the measurement's units (V, A, Hz, Ω, and so on). |
|
Configure DC voltage measurements using the 10 V range with 1 mV resolution.Then make and read one measurement: Typical Response:+8.54530000E+01 |
Sets all measurement parameters and trigger parameters to their default values for DC voltage ratio measurements and immediately triggers a measurement. The results are sent directly to the instrument's output buffer.
To calculate a ratio, the instrument measures a DC reference voltage applied to the Sense terminal and the DC signal voltage applied to the Input terminals. It then uses the formula:
Ratio = DC signal voltage / DC reference voltage
Parameter | Typical Return |
---|---|
<range>: 100 mV, 1 V, 10 V, 100 V, 1000 V, AUTO (default) or DEFault |
(none) |
<resolution>: See Resolution Table or Range, Resolution and NPLC. The default is equivalent to 10 PLC. |
|
Configure DC voltage ratio measurements using the 100 V range with 1 mV resolution. Then make and read one measurement: Typical Response:+4.27150000E+00 |