Waits for measurements to complete and copies all available measurements to the instrument's output buffer. The readings remain in reading memory.
Parameter | Typical Return |
---|---|
(none) | (none) |
Use FETCh? with CONFigure and INITiate. The INITiate command places the instrument in the "wait-for-trigger" state, triggers a measurement when the rear-panel Ext Trig input is pulsed (low by default), and sends the measurement to reading memory. The FETCh? query transfers the measurement from reading memory to the instrument's output buffer. CONF:VOLT:DC 10,0.003 Typical Response: -4.98748741E-01,-4.35163427E-01,-4.33118686E-01,-3.48109378E-01 |