Selects the slope of the voltmeter complete output signal on the rear-panel VM Comp BNC connector.
Parameter | Typical Return |
---|---|
{POSitive|NEGative}. Default: NEG | POS or NEG |
Configure DC voltage measurements and make two measurements. The signal on the rear-panel VM Comp connector outputs a positive pulse as each measurement is completed: CONF:VOLT:DC 10 |