The SYSTem subsystem includes general instrument configuration commands, I/O locking commands, license management commands, and remote interface configuration commands (listed below).
SYSTem:COMMunicate:GPIB:ADDRess
SYSTem:COMMunicate:LAN:CONTrol?
SYSTem:COMMunicate:LAN:DNS[{1|2}]
SYSTem:COMMunicate:LAN:DOMain?
SYSTem:COMMunicate:LAN:GATeway
SYSTem:COMMunicate:LAN:HOSTname
SYSTem:COMMunicate:LAN:IPADdress
SYSTem:COMMunicate:LAN:TELNet:PROMpt
SYSTem:COMMunicate:LAN:TELNet:WMESsage
SYSTem:COMMunicate:LAN:WINS[{1|2}]
Disables or enables the GPIB, USB, or LAN remote interface. Also disables or enables available remote services such as Sockets, HiSLIP, Telnet, VXI11, and the built-in Web Interface.
|
The GPIB interface is an optional feature. See Models and Options for details. |
Parameter | Typical Return |
---|---|
{ON|1|OFF|0}. Default: ON. for all interfaces | 0 (OFF) or 1 (ON) |
<interface>: {GPIB|HISLip|USB|LAN|SOCKets|TELNet|VXI11|WEB|USBMtp|USBHost} | |
Disable the USB interface: |
Assigns instrument's GPIB (IEEE-488) address, which is displayed at power-on. Each device on the GPIB interface must have a unique address.
|
The GPIB interface is an optional feature. See Models and Options for details. |
Parameter | Typical Return |
---|---|
0 to 30, default 22 | +15 |
Set GPIB address to 15: SYST:COMM:GPIB:ADDR 15 |
Reads the initial Control connection port number for Sockets communications. This connection is used to send and receive commands and queries.
Parameter | Typical Return |
---|---|
(none) | 5000 (0 if the interface does not support sockets) |
Return the Control connection port number: SYST:COMM:LAN:CONT? |
Disables or enables instrument's use of DHCP. The acronym DHCP stands for Dynamic Host Configuration Protocol, a protocol for assigning dynamic IP addresses to networked devices. With dynamic addressing, a device can have a different IP address every time it connects to the network.
ON: instrument tries to obtain an IP address from a DHCP server. If a DHCP server is found, it assigns a dynamic IP address, Subnet Mask, and Default Gateway to the instrument.
OFF or DHCP unavailable: instrument uses the static IP address, Subnet Mask, and Default Gateway during power-on.
|
If you change this setting, you must send SYSTem:COMMunicate:LAN:UPDate to activate the new setting. |
Parameter | Typical Return |
---|---|
{ON|1|OFF|0}. Default: ON. | 0 (OFF) or 1 (ON) |
Disable DHCP: SYST:COMM:LAN:DHCP OFF SYST:COMM:LAN:UPDate |
Assigns static IP addresses of Domain Name System (DNS) servers. A primary and a secondary server address may be assigned. If DHCP is available and enabled, DHCP will auto-assign these server addresses. These auto-assigned server addresses take precedence over the static addresses assigned with this command. Contact your LAN administrator for details.
|
If you change this setting, you must send SYSTem:COMMunicate:LAN:UPDate to activate the new setting. |
Parameter | Typical Return |
---|---|
Command: "nnn.nnn.nnn.nnn". Default: "0.0.0.0". Query: {CURRent|STATic}. Default: CURRent. |
"198.105.232.4" |
Set a static primary DNS address: SYST:COMM:LAN:DNS "198.105.232.4" SYST:COMM:LAN:UPD |
Returns the domain name assigned to the instrument.
Parameter | Typical Return |
---|---|
(none) | "example.com" |
Return the domain name being used by the instrument: SYST:COMM:LAN:DOM? |
Assigns a default gateway for the instrument. The specified IP Address sets the default gateway, which allows the instrument to communicate with systems that are not on the local subnet. Thus, this is the default gateway where packets are sent that are destined for a device not on the local subnet, as determined by the Subnet Mask setting. Contact your LAN administrator for details.
|
If you change this setting, you must send SYSTem:COMMunicate:LAN:UPDate to activate the new setting. |
Parameter | Typical Return |
---|---|
Command: "nnn.nnn.nnn.nnn". Default: "0.0.0.0". Query: {CURRent|STATic}. Default: CURRent. |
"198.105.232.1" |
Set default gateway address: SYST:COMM:LAN:GATEWAY "198.105.232.1" SYST:COMM:LAN:UPD |
Assigns a hostname to the instrument. A hostname is the host portion of the domain name, which is translated into an IP address. If Dynamic Domain Name System (Dynamic DNS) is available on your network and your instrument uses DHCP, the hostname is registered with the Dynamic DNS service at power-on. If DHCP is enabled (SYSTem:COMMunicate:LAN:DHCP ON), the DHCP server can change the specified hostname.
|
If you change this setting, you must send SYSTem:COMMunicate:LAN:UPDate to activate the new setting. |
Parameter | Typical Return |
---|---|
String of up to 15 characters. Default: "K-<instrument model number>-nnnnn", where nnnnn is the last five digits of the instrument's serial number. |
"LAB1-34461A" |
Define a hostname: |
Assigns a static Internet Protocol (IP) address for the instrument. If DHCP is enabled (SYSTem:COMMunicate:LAN:DHCP ON), the specified static IP address is not used. Contact your LAN administrator for details.
|
If you change this setting, you must send SYSTem:COMMunicate:LAN:UPDate to activate the new setting. |
Parameter | Typical Return |
---|---|
Command: "nnn.nnn.nnn.nnn" Query: {CURRent|STATic}. Default: CURRent. |
"169.254.149.35" |
Set a static IP address: SYST:COMM:LAN:IPAD "169.254.149.35" SYST:COMM:LAN:UPD |
Returns the instrument's Media Access Control (MAC) address as an ASCII string of 12 hexadecimal characters (0-9 and A-F) enclosed in quotation marks.
Your LAN administrator may need the MAC address to assign a static IP address for this device. |
Parameter | Typical Return |
---|---|
(none) | "0030D3001041" |
Return the MAC address: SYST:COMM:LAN:MAC? |
Assigns a subnet mask for the instrument to use in determining whether a client IP address is on the same local subnet. When a client IP address is on a different subnet, all packets must be sent to the Default Gateway. Contact your LAN administrator for details.
|
If you change this setting, you must send SYSTem:COMMunicate:LAN:UPDate to activate the new setting. |
Parameter | Typical Return |
---|---|
Command: "nnn.nnn.nnn.nnn". Default: "255.255.0.0". Query: {CURRent|STATic}. Default: CURRent. |
"255.255.255.0" |
Set the subnet mask: SYST:COMM:LAN:SMAS "255.255.255.0" SYST:COMM:LAN:UPD |
Sets the command prompt seen when communicating with the instrument via Telnet.
Parameter | Typical Return |
---|---|
String of up to 15 characters Default is Instrument Model Number: 34460A>, 34461A>, 34465A>, or 34470A> |
"Command>" |
Set the command prompt: SYST:COMM:LAN:TELN:PROM "Command>" |
Sets welcome message seen when communicating with instrument via Telnet.
Parameter | Typical Return |
---|---|
Quoted string of up to 63 characters. Default: "Welcome to Keysight's <instrument model number> Digital Multimeter" |
"Welcome to the Telnet Session" |
Define a welcome message: |
Stores any changes made to the LAN settings into non-volatile memory and restarts the LAN driver with the updated settings.
Parameter | Typical Return |
---|---|
(none) | (none) |
(see below) |
The following example configures the instrument to use statically assigned LAN settings.
SYST:COMM:LAN:DHCP OFF
SYST:COMM:LAN:DNS "198.105.232.4"
SYST:COMM:LAN:DNS2 "198.105.232.5"
SYST:COMM:LAN:GAT "198.105.232.1"
SYST:COMM:LAN:HOST "LAB1-DMM"
SYST:COMM:LAN:IPAD "198.105.232.101"
SYST:COMM:LAN:SMAS "255.255.255.0"
SYST:COMM:LAN:WINS "198.105.232.4"
SYST:COMM:LAN:WINS "198.105.232.5"
SYST:COMM:LAN:UPD
The following example configures the instrument back to use DHCP.
SYST:COMM:LAN:DHCP ON
SYST:COMM:LAN:UPD
Assigns the static IP addresses of the Windows Internet Name System (WINS) servers. A primary and a secondary server address may be assigned. If DHCP is available and enabled, DHCP will auto-assign these server addresses. These auto-assigned server addresses take precedence over the static addresses assigned with this command. Contact your LAN administrator for details.
|
If you change this setting, you must send SYSTem:COMMunicate:LAN:UPDate to activate the new setting. |
Parameter | Typical Return |
---|---|
Command: "nnn.nnn.nnn.nnn". Default: "0.0.0.0". Query: {CURRent|STATic}. Default: CURRent. |
"198.105.232.4" |
Set a static primary WINS address: SYST:COMM:LAN:WINS "198.105.232.4" SYST:COMM:LAN:UPD |
Disables or enables the front panel USB host port. Calibration security must be unsecured (CALibration:SECure:STATe <code>,OFF) before sending this command.
Parameter | Typical Return |
---|---|
{ON|1|OFF|0}. Default: OFF. | 0 (OFF) or 1 (ON) |
Disable the USB host port:
|